<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB device design question in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-device-design-question/m-p/523502#M6138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by djbuijs on Wed May 21 16:35:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a product with an LPC1788 which needs the following USB features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Firmware upgrade over USB (from host PC to device, [u]not[/u] through a USB key).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- File upload from the device to the host.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- [optional] Ideally we'd also be able to get some information from the device like serial number etc, but this is not critical.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The device should only work with a custom program, so simply using a mass-storage device as-is will not do. There are quite a lot of data to upload (200MB +), so using USB bulk transfers seem necessary to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the best way to approach this? I was hoping to use nxpUSBlib or winUSB, so I don't have to go through the Windows driver validation process. What are my options? Is there some way to make the mass-storage device invisible for Windows? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I appreciate your input!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dirk&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:44:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:44:33Z</dc:date>
    <item>
      <title>USB device design question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-device-design-question/m-p/523502#M6138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by djbuijs on Wed May 21 16:35:30 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a product with an LPC1788 which needs the following USB features:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Firmware upgrade over USB (from host PC to device, [u]not[/u] through a USB key).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- File upload from the device to the host.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- [optional] Ideally we'd also be able to get some information from the device like serial number etc, but this is not critical.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The device should only work with a custom program, so simply using a mass-storage device as-is will not do. There are quite a lot of data to upload (200MB +), so using USB bulk transfers seem necessary to me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is the best way to approach this? I was hoping to use nxpUSBlib or winUSB, so I don't have to go through the Windows driver validation process. What are my options? Is there some way to make the mass-storage device invisible for Windows? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I appreciate your input!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dirk&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-device-design-question/m-p/523502#M6138</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:33Z</dc:date>
    </item>
    <item>
      <title>Re: USB device design question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-device-design-question/m-p/523503#M6139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri May 23 12:42:18 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Dirk,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Maybe this USB secondary bootloader application note will help you:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Fan10866-lpc1700-secondary-usb-bootloader" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/an10866-lpc1700-secondary-usb-bootloader&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-device-design-question/m-p/523503#M6139</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:34Z</dc:date>
    </item>
  </channel>
</rss>