<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC4337 Two usb host</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-Two-usb-host/m-p/523452#M6088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Fri Apr 04 10:24:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes it is possible. The LPC4337 has two independent high speed USB controllers that both support host mode. Each of these controllers has its own dedicated port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note that the internal PHY on USB1 only supports full speed operation but this controller does have a ULPI interface which you can connect to an external high speed PHY.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:44:35 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:44:35Z</dc:date>
    <item>
      <title>LPC4337 Two usb host</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-Two-usb-host/m-p/523451#M6087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by snovik on Thu Apr 03 00:06:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) I tried this project (&lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com/content/project/Dual-USB-Host-Device-solution"&gt;NXP Dual USB Solution&lt;/A&gt;&lt;SPAN&gt;), It works fine. I need to implement the same, only use the second usb flash instead of sd card (Copying the contents usb1 flash on usb2 flash).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to use two ports usb lpc4337 as hosts together?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-Two-usb-host/m-p/523451#M6087</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 Two usb host</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-Two-usb-host/m-p/523452#M6088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drs on Fri Apr 04 10:24:07 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes it is possible. The LPC4337 has two independent high speed USB controllers that both support host mode. Each of these controllers has its own dedicated port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note that the internal PHY on USB1 only supports full speed operation but this controller does have a ULPI interface which you can connect to an external high speed PHY.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-Two-usb-host/m-p/523452#M6088</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:35Z</dc:date>
    </item>
  </channel>
</rss>