<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックreading/writing SDCARD using USB</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-writing-SDCARD-using-USB/m-p/523410#M6046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GuusReijnders_CG on Tue Jul 29 05:19:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the development board MCB1800 (lp1856) from Keil.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can compile and the examples usb_rom_msc_ram and periph_sdmmc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But the first example uses RAM instead of an SDCARD, so I want to combine these two examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can read the number of sector and size of the SDCARD, so I can set the right settings for USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In windows the right size of the SDCARD is shown.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But now I want to read and write the Card using USB. I see the functions translate_rd and translate_wr.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried several things but nothing is working yet. What code do I need to add to let the SDCARD work with USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen the gunctions diskr_read and disk_write. However when I use these functions in the USB routines the application gangs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:46:27 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:46:27Z</dc:date>
    <item>
      <title>reading/writing SDCARD using USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-writing-SDCARD-using-USB/m-p/523410#M6046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GuusReijnders_CG on Tue Jul 29 05:19:43 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the development board MCB1800 (lp1856) from Keil.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can compile and the examples usb_rom_msc_ram and periph_sdmmc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But the first example uses RAM instead of an SDCARD, so I want to combine these two examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can read the number of sector and size of the SDCARD, so I can set the right settings for USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In windows the right size of the SDCARD is shown.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But now I want to read and write the Card using USB. I see the functions translate_rd and translate_wr.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried several things but nothing is working yet. What code do I need to add to let the SDCARD work with USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen the gunctions diskr_read and disk_write. However when I use these functions in the USB routines the application gangs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/reading-writing-SDCARD-using-USB/m-p/523410#M6046</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: reading/writing SDCARD using USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/reading-writing-SDCARD-using-USB/m-p/523411#M6047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Fri Aug 08 15:29:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, GuusReijnders_CG,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please visit the second demonstration/implementation at below solution page for interfacing SDCARD with USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fproject%2FDual-USB-Host-Device-solution" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/project/Dual-USB-Host-Device-solution&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/reading-writing-SDCARD-using-USB/m-p/523411#M6047</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:46:28Z</dc:date>
    </item>
  </channel>
</rss>