<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4088 pendrive support in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-pendrive-support/m-p/2419414#M59824</link>
    <description>&lt;P&gt;Hello. I am implementing USB Host functionality on the LPC4088 for pendrive support. The code works correctly on the LPC QuickStart board, but fails to enumerate devices on our custom hardware.&lt;BR /&gt;Specifically, `USB_Host_SendControlRequest()` returns `HOST_SENDCONTROL_PipeError` instead of `HOST_SENDCONTROL_Successful` during enumeration. I suspect the issue lies within `HcdControlTransfer()`, possibly related to pipe configuration, but I have been unable to identify the root cause.&lt;BR /&gt;Any insights would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Oct 2026 09:42:36 GMT</pubDate>
    <dc:creator>Nipperkin</dc:creator>
    <dc:date>2026-10-08T09:42:36Z</dc:date>
    <item>
      <title>LPC4088 pendrive support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-pendrive-support/m-p/2419414#M59824</link>
      <description>&lt;P&gt;Hello. I am implementing USB Host functionality on the LPC4088 for pendrive support. The code works correctly on the LPC QuickStart board, but fails to enumerate devices on our custom hardware.&lt;BR /&gt;Specifically, `USB_Host_SendControlRequest()` returns `HOST_SENDCONTROL_PipeError` instead of `HOST_SENDCONTROL_Successful` during enumeration. I suspect the issue lies within `HcdControlTransfer()`, possibly related to pipe configuration, but I have been unable to identify the root cause.&lt;BR /&gt;Any insights would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2026 09:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-pendrive-support/m-p/2419414#M59824</guid>
      <dc:creator>Nipperkin</dc:creator>
      <dc:date>2026-10-08T09:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 pendrive support</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-pendrive-support/m-p/2420029#M59826</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/267212"&gt;@Nipperkin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Since the same firmware works on the LPC4088 QuickStart board, the issue is likely hardware-related rather than in HcdControlTransfer() itself. I would recommend checking:&lt;/P&gt;
&lt;P&gt;USB VBUS 5V power and power-switch control&lt;BR /&gt;D+/D− routing and pin configuration&lt;BR /&gt;USB 48 MHz clock configuration&lt;BR /&gt;Placement/alignment of USB Host DMA structures (HCCA/ED/TD) in USB-accessible RAM&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Sat, 10 Oct 2026 03:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-pendrive-support/m-p/2420029#M59826</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-10-10T03:01:45Z</dc:date>
    </item>
  </channel>
</rss>