<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHuge power consumption on RTC ofLPCXpresso54S018M EVB.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Huge-power-consumption-on-RTC-ofLPCXpresso54S018M-EVB/m-p/2415922#M59805</link>
    <description>&lt;P&gt;I use are LPCXpresso54S018M EVB. I need the RTC in the LPC54018 to work after the main power supply is removed. I initialized and enabled the RTC in my firmware. I powered the VBATT line (J10:11) with a coin cell battery CR2032. While the main power is present, the VBATT line consumption is == 0. It's Ok. However, after removing the main power supply, the VBATT line consumption increases up to ~41 uA! According to the datasheet, consumption should be less than 1 uA. Why? How can I achieve current consumption of 1 µA or less?&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2026 07:44:48 GMT</pubDate>
    <dc:creator>jcxz</dc:creator>
    <dc:date>2026-09-24T07:44:48Z</dc:date>
    <item>
      <title>Huge power consumption on RTC ofLPCXpresso54S018M EVB.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Huge-power-consumption-on-RTC-ofLPCXpresso54S018M-EVB/m-p/2415922#M59805</link>
      <description>&lt;P&gt;I use are LPCXpresso54S018M EVB. I need the RTC in the LPC54018 to work after the main power supply is removed. I initialized and enabled the RTC in my firmware. I powered the VBATT line (J10:11) with a coin cell battery CR2032. While the main power is present, the VBATT line consumption is == 0. It's Ok. However, after removing the main power supply, the VBATT line consumption increases up to ~41 uA! According to the datasheet, consumption should be less than 1 uA. Why? How can I achieve current consumption of 1 µA or less?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2026 07:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Huge-power-consumption-on-RTC-ofLPCXpresso54S018M-EVB/m-p/2415922#M59805</guid>
      <dc:creator>jcxz</dc:creator>
      <dc:date>2026-09-24T07:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: Huge power consumption on RTC ofLPCXpresso54S018M EVB.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Huge-power-consumption-on-RTC-ofLPCXpresso54S018M-EVB/m-p/2416685#M59810</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263728"&gt;@jcxz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The ~41 µA is most likely leakage through the RESETN circuitry , not RTC consumption. When main power is removed, VBAT &amp;gt; VDD; If VBAT&amp;gt; VDD, the external reset pin must be floating to prevent high VBAT leakage.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1790587431293.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396945i4208E634E4381113/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1790587431293.png" alt="Harry_Zhang_0-1790587431293.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The LPCXpresso54S018M-EVK connects RESETN to its pushbutton/debug circuitry, so the unmodified EVK does not satisfy that measurement condition.&lt;/P&gt;
&lt;P&gt;To reduce the current:&lt;/P&gt;
&lt;P&gt;Isolate the MCU’s RESETN pin from the EVK reset network.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 09:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Huge-power-consumption-on-RTC-ofLPCXpresso54S018M-EVB/m-p/2416685#M59810</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-09-28T09:24:03Z</dc:date>
    </item>
  </channel>
</rss>