<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB Mass Storage Device - Embedded Artist DevKit LPC1788</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Device-Embedded-Artist-DevKit-LPC1788/m-p/523344#M5980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by grieto on Tue Nov 12 14:27:37 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm in the process of evaluating/prototyping with the EA1788 for an embedded design.&amp;nbsp; I have been leveraging off of the examples provided in LPCOpen v1.03.&amp;nbsp; I have successfully compiled a ran several of the examples for the EA1788 platform including the Mass Storage Device example using RAM.&amp;nbsp; However, I would like to evaluate the Mass Storage Device example using an SD card instead of RAM.&amp;nbsp; Reading through the literature and code, I see mention of defining CFG_SDCARD to enable this option.&amp;nbsp; However, when I do this I have many issues compiling for the code.&amp;nbsp; Troubleshooting some of the compile issues, I realized the core code for the LPC18xx (Hitex EVA 1850) seemed to have most of the code there to build correctly... I think it built with only 3 errors.&amp;nbsp; So, I'm wondering if there is a working version of the Mass Storage Device example using an SD card for the Embedded Artist 1788 devKit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help would be appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, Greg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:42:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:42:49Z</dc:date>
    <item>
      <title>USB Mass Storage Device - Embedded Artist DevKit LPC1788</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Device-Embedded-Artist-DevKit-LPC1788/m-p/523344#M5980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by grieto on Tue Nov 12 14:27:37 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm in the process of evaluating/prototyping with the EA1788 for an embedded design.&amp;nbsp; I have been leveraging off of the examples provided in LPCOpen v1.03.&amp;nbsp; I have successfully compiled a ran several of the examples for the EA1788 platform including the Mass Storage Device example using RAM.&amp;nbsp; However, I would like to evaluate the Mass Storage Device example using an SD card instead of RAM.&amp;nbsp; Reading through the literature and code, I see mention of defining CFG_SDCARD to enable this option.&amp;nbsp; However, when I do this I have many issues compiling for the code.&amp;nbsp; Troubleshooting some of the compile issues, I realized the core code for the LPC18xx (Hitex EVA 1850) seemed to have most of the code there to build correctly... I think it built with only 3 errors.&amp;nbsp; So, I'm wondering if there is a working version of the Mass Storage Device example using an SD card for the Embedded Artist 1788 devKit?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help would be appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, Greg&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-Mass-Storage-Device-Embedded-Artist-DevKit-LPC1788/m-p/523344#M5980</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:42:49Z</dc:date>
    </item>
  </channel>
</rss>