<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: WS2812 interface With LPC5514JBD64E</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2405193#M59735</link>
    <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265217"&gt;@Kishore02&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The WS2812 protocol requires a precisely timed single-wire digital output signal. Therefore, the DIN signal should preferably be generated by a timer/PWM peripheral rather than by software bit-banging.&lt;/P&gt;
&lt;P&gt;For LPC551x devices, one practical solution is to use an SCTimer output.&lt;/P&gt;
&lt;P&gt;The exact pin depends on your hardware design and pin mux configuration. Any pin that can be configured as an SCTimer output can potentially be used.&lt;/P&gt;
&lt;P&gt;For example, the LPC55S16 SDK provides the sctimer_pwm_with_dutycycle_change example, which uses:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;SCT0_OUT2  (J12-12 on LPCXpresso55S16 board)&lt;/LI-CODE&gt;
&lt;P&gt;2.&amp;nbsp;Since the LPC5514 operates at 3.3 V logic and the WS2812 is typically powered from 5 V, level shifting is recommended to improve signal integrity and ensure reliable operation.&lt;/P&gt;
&lt;P&gt;3.&amp;nbsp;Yes.&lt;/P&gt;
&lt;P&gt;A 74AHCT125 is a commonly used and recommended solution for interfacing a 3.3 V MCU with a 5 V WS2812 device.&lt;/P&gt;
&lt;P&gt;4.&amp;nbsp;For LPC551x devices, the preferred approaches would be:&lt;/P&gt;
&lt;P&gt;SCTimer (recommended)&lt;/P&gt;
&lt;P&gt;Generate an 800 kHz waveform.&lt;BR /&gt;Dynamically update the PWM duty cycle for each transmitted bit.&lt;BR /&gt;Similar to the SDK example:&lt;/P&gt;
&lt;P&gt;sctimer_pwm_with_dutycycle_change&lt;/P&gt;
&lt;P&gt;5.At the moment, I am not aware of an official MCUXpresso SDK example specifically targeting WS2812 or NeoPixel LEDs for the LPC5514.&lt;/P&gt;
&lt;P&gt;However, the SDK does provide several SCTimer PWM examples that can be used as a starting point.&lt;/P&gt;
&lt;P&gt;In particular:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;sctimer_pwm
sctimer_pwm_with_dutycycle_change&lt;/LI-CODE&gt;
&lt;P&gt;Although I have not found a dedicated WS2812 example for the LPC5514 SDK, I previously achieved reliable WS2812 control on the FRDM-MCXN947 board using an SCTimer + eDMA solution.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;6.&amp;nbsp;I would recommend starting from:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;lpcxpresso55s16_sctimer_pwm_with_dutycycle_change
&lt;/LI-CODE&gt;
&lt;P&gt;7.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The recommended development environment is:&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE&lt;BR /&gt;MCUXpresso SDK&lt;BR /&gt;LPC-Link2 or MCU-Link debugger&lt;BR /&gt;On-board CMSIS-DAP debugger (if available on the evaluation board)&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
    <pubDate>Fri, 14 Aug 2026 09:28:51 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2026-08-14T09:28:51Z</dc:date>
    <item>
      <title>WS2812 interface With LPC5514JBD64E</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2403976#M59734</link>
      <description>&lt;P&gt;Hi NXP Community,&lt;/P&gt;&lt;P&gt;I am working with an LPC5514JBD64E-based controller and I need to interface a WS2812/WS2812B LED ring with the MCU.&lt;/P&gt;&lt;P&gt;I am studying the LPC5514JBD64E datasheet and my controller schematic, but I am new to the LPC55xx family and need some guidance.&lt;/P&gt;&lt;P&gt;I would like to know:&lt;/P&gt;&lt;P&gt;1. Which GPIO pin of the LPC5514JBD64E should be used for the WS2812 data (DIN) signal?&lt;/P&gt;&lt;P&gt;2. Since the LPC5514JBD64E uses 3.3 V logic and the WS2812 will be powered from 5 V, what is the recommended hardware connection between the MCU and WS2812?&lt;/P&gt;&lt;P&gt;3. Is a 74AHCT125 recommended between the MCU GPIO and WS2812 DIN?&lt;/P&gt;&lt;P&gt;4. Which peripheral or method should be used to generate the precise timing required by the WS2812 protocol?&lt;/P&gt;&lt;P&gt;5. Is there an official NXP SDK example, driver, or sample code for controlling WS2812 or NeoPixel LEDs using the LPC5514JBD64E?&lt;/P&gt;&lt;P&gt;6. If there is no WS2812-specific example, could you provide or point me to a basic working example code that makes a WS2812 LED or LED ring blink or change color?&lt;/P&gt;&lt;P&gt;7. What is the recommended development environment and programming/debugging procedure for this MCU?&lt;/P&gt;&lt;P&gt;My immediate goal is to make the WS2812 LED ring blink and display different colors using the LPC5514JBD64E.&lt;/P&gt;&lt;P&gt;I would appreciate guidance on the correct GPIO, hardware connection, peripheral, and example code.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 12 Aug 2026 06:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2403976#M59734</guid>
      <dc:creator>Kishore02</dc:creator>
      <dc:date>2026-08-12T06:31:06Z</dc:date>
    </item>
    <item>
      <title>Re: WS2812 interface With LPC5514JBD64E</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2405193#M59735</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/265217"&gt;@Kishore02&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The WS2812 protocol requires a precisely timed single-wire digital output signal. Therefore, the DIN signal should preferably be generated by a timer/PWM peripheral rather than by software bit-banging.&lt;/P&gt;
&lt;P&gt;For LPC551x devices, one practical solution is to use an SCTimer output.&lt;/P&gt;
&lt;P&gt;The exact pin depends on your hardware design and pin mux configuration. Any pin that can be configured as an SCTimer output can potentially be used.&lt;/P&gt;
&lt;P&gt;For example, the LPC55S16 SDK provides the sctimer_pwm_with_dutycycle_change example, which uses:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;SCT0_OUT2  (J12-12 on LPCXpresso55S16 board)&lt;/LI-CODE&gt;
&lt;P&gt;2.&amp;nbsp;Since the LPC5514 operates at 3.3 V logic and the WS2812 is typically powered from 5 V, level shifting is recommended to improve signal integrity and ensure reliable operation.&lt;/P&gt;
&lt;P&gt;3.&amp;nbsp;Yes.&lt;/P&gt;
&lt;P&gt;A 74AHCT125 is a commonly used and recommended solution for interfacing a 3.3 V MCU with a 5 V WS2812 device.&lt;/P&gt;
&lt;P&gt;4.&amp;nbsp;For LPC551x devices, the preferred approaches would be:&lt;/P&gt;
&lt;P&gt;SCTimer (recommended)&lt;/P&gt;
&lt;P&gt;Generate an 800 kHz waveform.&lt;BR /&gt;Dynamically update the PWM duty cycle for each transmitted bit.&lt;BR /&gt;Similar to the SDK example:&lt;/P&gt;
&lt;P&gt;sctimer_pwm_with_dutycycle_change&lt;/P&gt;
&lt;P&gt;5.At the moment, I am not aware of an official MCUXpresso SDK example specifically targeting WS2812 or NeoPixel LEDs for the LPC5514.&lt;/P&gt;
&lt;P&gt;However, the SDK does provide several SCTimer PWM examples that can be used as a starting point.&lt;/P&gt;
&lt;P&gt;In particular:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;sctimer_pwm
sctimer_pwm_with_dutycycle_change&lt;/LI-CODE&gt;
&lt;P&gt;Although I have not found a dedicated WS2812 example for the LPC5514 SDK, I previously achieved reliable WS2812 control on the FRDM-MCXN947 board using an SCTimer + eDMA solution.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;6.&amp;nbsp;I would recommend starting from:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;lpcxpresso55s16_sctimer_pwm_with_dutycycle_change
&lt;/LI-CODE&gt;
&lt;P&gt;7.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The recommended development environment is:&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE&lt;BR /&gt;MCUXpresso SDK&lt;BR /&gt;LPC-Link2 or MCU-Link debugger&lt;BR /&gt;On-board CMSIS-DAP debugger (if available on the evaluation board)&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 14 Aug 2026 09:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2405193#M59735</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-08-14T09:28:51Z</dc:date>
    </item>
    <item>
      <title>Re: WS2812 interface With LPC5514JBD64E</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2405302#M59736</link>
      <description>Can you please provide the code for this project?</description>
      <pubDate>Fri, 14 Aug 2026 12:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/WS2812-interface-With-LPC5514JBD64E/m-p/2405302#M59736</guid>
      <dc:creator>Kishore02</dc:creator>
      <dc:date>2026-08-14T12:46:46Z</dc:date>
    </item>
  </channel>
</rss>