<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1778 can't connect after programming by JLINK</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-can-t-connect-after-programming-by-JLINK/m-p/2376317#M59588</link>
    <description>&lt;P&gt;Hello! After programming the LPC1778 chip with a J-Link debugger, the target chip cannot be connected. This same fault has happened on two distinct circuit boards in my possession.&lt;/P&gt;&lt;P&gt;I confirm the issue is not caused by the programmed application code. The data I programmed is full-chip random values, and programming the exact same random dataset using a different programming tool does not produce this connectivity issue.&lt;/P&gt;&lt;P&gt;The initial connection and programming process complete normally without any error alerts. After power cycling the board post-programming, all communication with the hardware fails. The connection log is listed below:&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;- Connecting via USB to probe/ programmer device 0&lt;BR /&gt;- Probe/ Programmer firmware: J-Link V9 compiled May 7 2021 16:26:12&lt;BR /&gt;- Probe/ Programmer S/N: 69401860&lt;BR /&gt;- Device "LPC1778" selected.&lt;BR /&gt;- Target interface speed: 4000 kHz (Fixed)&lt;BR /&gt;- VTarget = 3.283V&lt;BR /&gt;- Failed to attach to CPU. Trying connect under reset.&lt;BR /&gt;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;BR /&gt;General troubleshooting guide: &lt;A href="https://kb.segger.com/J-Link_Troubleshooting" target="_blank"&gt;https://kb.segger.com/J-Link_Troubleshooting&lt;/A&gt;&lt;BR /&gt;- ERROR: Connect failed&lt;/P&gt;&lt;P&gt;Addtionally, I capture waveforms with a logic analyzer, the DP port of the SWD interface works normally, whereas all AP accesses result in ACK FAULT responses.&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jun 2026 01:55:34 GMT</pubDate>
    <dc:creator>BianHaopeng1</dc:creator>
    <dc:date>2026-06-04T01:55:34Z</dc:date>
    <item>
      <title>LPC1778 can't connect after programming by JLINK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-can-t-connect-after-programming-by-JLINK/m-p/2376317#M59588</link>
      <description>&lt;P&gt;Hello! After programming the LPC1778 chip with a J-Link debugger, the target chip cannot be connected. This same fault has happened on two distinct circuit boards in my possession.&lt;/P&gt;&lt;P&gt;I confirm the issue is not caused by the programmed application code. The data I programmed is full-chip random values, and programming the exact same random dataset using a different programming tool does not produce this connectivity issue.&lt;/P&gt;&lt;P&gt;The initial connection and programming process complete normally without any error alerts. After power cycling the board post-programming, all communication with the hardware fails. The connection log is listed below:&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;- Connecting via USB to probe/ programmer device 0&lt;BR /&gt;- Probe/ Programmer firmware: J-Link V9 compiled May 7 2021 16:26:12&lt;BR /&gt;- Probe/ Programmer S/N: 69401860&lt;BR /&gt;- Device "LPC1778" selected.&lt;BR /&gt;- Target interface speed: 4000 kHz (Fixed)&lt;BR /&gt;- VTarget = 3.283V&lt;BR /&gt;- Failed to attach to CPU. Trying connect under reset.&lt;BR /&gt;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;BR /&gt;General troubleshooting guide: &lt;A href="https://kb.segger.com/J-Link_Troubleshooting" target="_blank"&gt;https://kb.segger.com/J-Link_Troubleshooting&lt;/A&gt;&lt;BR /&gt;- ERROR: Connect failed&lt;/P&gt;&lt;P&gt;Addtionally, I capture waveforms with a logic analyzer, the DP port of the SWD interface works normally, whereas all AP accesses result in ACK FAULT responses.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 01:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-can-t-connect-after-programming-by-JLINK/m-p/2376317#M59588</guid>
      <dc:creator>BianHaopeng1</dc:creator>
      <dc:date>2026-06-04T01:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 can't connect after programming by JLINK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-can-t-connect-after-programming-by-JLINK/m-p/2376399#M59589</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262795"&gt;@BianHaopeng1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;Please first download and run a simple “Hello World” project on your board, rather than using random values, and then test whether debugging works properly.&lt;/P&gt;
&lt;P&gt;If debugging still does not work, please check your schematic design by referring to the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/OM13085" target="_blank"&gt;LPCXpresso board for LPC1769 with CMSIS DAP probe | NXP Semiconductors&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;If the issue still persists, please feel free to contact me.&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Thu, 04 Jun 2026 04:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-can-t-connect-after-programming-by-JLINK/m-p/2376399#M59589</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2026-06-04T04:07:53Z</dc:date>
    </item>
  </channel>
</rss>