<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: usb host with CODEC(i2S)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2305473#M59355</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259484"&gt;@harry3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post,&lt;/P&gt;
&lt;P&gt;There is not a solution that accomplishes with the requirements you mentioned, but you could use as reference the examples of host_audio_speaker it has the options of bm or freertos (Included in SDK_25.12.00_LPCXpresso55S28).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1770140902886.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375343i3683F07DD25D27F2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1770140902886.png" alt="carlos_o_0-1770140902886.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also, there are two examples of I2S one using DMA and the other using interrupts, please refer to these examples.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_1-1770141287616.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375344iAD9A0604E1FA7C7F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_1-1770141287616.png" alt="carlos_o_1-1770141287616.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;The final implementation is up to you, feel free to reach out with any questions in the&amp;nbsp;developing process of the solution.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 17:55:02 GMT</pubDate>
    <dc:creator>carlos_o</dc:creator>
    <dc:date>2026-02-03T17:55:02Z</dc:date>
    <item>
      <title>usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2305179#M59354</link>
      <description>&lt;P&gt;hi NXP team，&lt;/P&gt;&lt;P&gt;我使用LPC5528开发一个项目， lpc5528 I2S RX 接收来自外接的I2S tx信号，通过USB输出数字信号给usb扬声器。这需要用到USB HOST+i2s 的组件方案。但是我在例程中没有找到这样的方案。请问可以提供一个这样的方案吗？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm developing a project using LPC5528. The LPC5528 I2S RX receives I2S TX signals from an external device, and outputs digital signals to a USB speaker via USB. This requires a solution using USB HOST + I2S components. However, I couldn't find such a solution in the example code. Could you provide a solution like this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 09:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2305179#M59354</guid>
      <dc:creator>harry3</dc:creator>
      <dc:date>2026-02-03T09:37:48Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2305473#M59355</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259484"&gt;@harry3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post,&lt;/P&gt;
&lt;P&gt;There is not a solution that accomplishes with the requirements you mentioned, but you could use as reference the examples of host_audio_speaker it has the options of bm or freertos (Included in SDK_25.12.00_LPCXpresso55S28).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1770140902886.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375343i3683F07DD25D27F2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1770140902886.png" alt="carlos_o_0-1770140902886.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also, there are two examples of I2S one using DMA and the other using interrupts, please refer to these examples.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_1-1770141287616.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375344iAD9A0604E1FA7C7F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_1-1770141287616.png" alt="carlos_o_1-1770141287616.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;The final implementation is up to you, feel free to reach out with any questions in the&amp;nbsp;developing process of the solution.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 17:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2305473#M59355</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-02-03T17:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2313360#M59365</link>
      <description>&lt;P&gt;hi carlos&lt;BR /&gt;我现在开发这个项目遇到问题，我把CODEC的文件夹以及包含的文件拷贝到项目的目录下。在编译的时候总是提示在DEBUG文件夹没有找到我添加的文件夹。请问要添加文件夹需要怎么配置IDE呢？&lt;BR /&gt;I'm currently encountering a problem while developing this project. I copied the CODEC folder and its contained files into the project directory. During compilation, it always prompts that the folder I added cannot be found in the DEBUG folder. How do I need to configure the IDE to add the folder?&lt;/P&gt;&lt;P&gt;thanks&lt;BR /&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 04:06:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2313360#M59365</guid>
      <dc:creator>harry3</dc:creator>
      <dc:date>2026-02-06T04:06:44Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2313908#M59370</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259484"&gt;@harry3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please also at the codec path to the MCU Assembler settings&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1770396866380.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375924i4EC19ECAA36D92C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1770396866380.png" alt="carlos_o_0-1770396866380.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;let me know if this solves the issue.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 16:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2313908#M59370</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-02-06T16:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2314056#M59371</link>
      <description>&lt;P&gt;hi carlos,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;出这个问题的时候我已经是这样做的了。&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I had already done it this way when this problem arose.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;harry &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 07 Feb 2026 07:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2314056#M59371</guid>
      <dc:creator>harry3</dc:creator>
      <dc:date>2026-02-07T07:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2314874#M59376</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259484"&gt;@harry3&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for clarifying.&lt;/P&gt;
&lt;P&gt;Please also add the folder to Path and Symbols -&amp;gt; Source location to be recognized as a folder with source files:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1770659481917.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/376190i8D377DF089AA26AA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1770659481917.png" alt="carlos_o_0-1770659481917.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could confirm that the change make effect when the folder symbol has a blue C.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Feb 2026 17:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2314874#M59376</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-02-09T17:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2316006#M59381</link>
      <description>&lt;P&gt;hi Carlos，&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm very sorry that I made a mistake with the attachment just now. Please refer to this initial attachment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;harry&lt;/P&gt;</description>
      <pubDate>Wed, 11 Feb 2026 04:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2316006#M59381</guid>
      <dc:creator>harry3</dc:creator>
      <dc:date>2026-02-11T04:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: usb host with CODEC(i2S)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2316064#M59383</link>
      <description>&lt;P&gt;hi carlos,&lt;/P&gt;&lt;DIV class=""&gt;Thank you very much for your support.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;I just found the problem of MCLk having no output. I will further develop this project and will continue to consult you if I encounter any problems in the future.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;thanks&lt;/DIV&gt;&lt;DIV class=""&gt;harry&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Wed, 11 Feb 2026 06:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/usb-host-with-CODEC-i2S/m-p/2316064#M59383</guid>
      <dc:creator>harry3</dc:creator>
      <dc:date>2026-02-11T06:45:09Z</dc:date>
    </item>
  </channel>
</rss>