<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1754 USB mass storage in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1754-USB-mass-storage/m-p/2259174#M59060</link>
    <description>&lt;P&gt;I have designed a board with LPC1754 and connected a nor flash W25Q64 to it via spi. As the nor flash is not formatable to FAT16 with cmsis FileSystem, I used chan's FatFs in my project and added keil mdk usb device mass storage with cmsis driver. While connecting to pc shows device descriptor correctly and Ii is recognized as a mass storage device but windows can not specify number of disk sectors correctly. Formating and exploring it is not possible. I have formatted it within a firmware with f_mkfs function and I am almost sure that chan's FatFs works correctly in my project. I wonder to know if someone have any related experience?&lt;/P&gt;</description>
    <pubDate>Wed, 10 Dec 2025 11:31:24 GMT</pubDate>
    <dc:creator>jalilisahar</dc:creator>
    <dc:date>2025-12-10T11:31:24Z</dc:date>
    <item>
      <title>LPC1754 USB mass storage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1754-USB-mass-storage/m-p/2259174#M59060</link>
      <description>&lt;P&gt;I have designed a board with LPC1754 and connected a nor flash W25Q64 to it via spi. As the nor flash is not formatable to FAT16 with cmsis FileSystem, I used chan's FatFs in my project and added keil mdk usb device mass storage with cmsis driver. While connecting to pc shows device descriptor correctly and Ii is recognized as a mass storage device but windows can not specify number of disk sectors correctly. Formating and exploring it is not possible. I have formatted it within a firmware with f_mkfs function and I am almost sure that chan's FatFs works correctly in my project. I wonder to know if someone have any related experience?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Dec 2025 11:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1754-USB-mass-storage/m-p/2259174#M59060</guid>
      <dc:creator>jalilisahar</dc:creator>
      <dc:date>2025-12-10T11:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1754 USB mass storage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1754-USB-mass-storage/m-p/2259468#M59062</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253152"&gt;@jalilisahar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please refer to the application note FAT library EFSL and FatFs port on NXP LPC1700 (AN10916). This document describes, in a step-by-step manner, how to port FatFs to the LPC1700 series.&lt;/P&gt;
&lt;P&gt;Additionally, it provides sample software that has been tested on Keil’s MCB1700 evaluation board (LPC1768).&lt;/P&gt;
&lt;P&gt;You can find the application note in the documentation section of the LPC1754 product page.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Wed, 10 Dec 2025 20:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1754-USB-mass-storage/m-p/2259468#M59062</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-12-10T20:17:02Z</dc:date>
    </item>
  </channel>
</rss>