<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DAC VREF dependency in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-VREF-dependency/m-p/2249822#M59023</link>
    <description>&lt;P&gt;For minimum power, you can configure VREF in bandgap-only mode and disable unnecessary features. Buffering is not required if you are not using VREF_OUT as the DAC reference.&lt;BR /&gt;More details for VREF, please refer to the attached presentations on this post: &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-on-DAC-current-sources-ZTC-PTAT/m-p/2159839" target="_blank"&gt;LPC5536: on DAC current sources (ZTC, PTAT)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 22:36:29 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2025-11-26T22:36:29Z</dc:date>
    <item>
      <title>DAC VREF dependency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-VREF-dependency/m-p/2247498#M59010</link>
      <description>&lt;P&gt;Using LPC553x for a low power application.&amp;nbsp; Reference Manual Rev 3, 07/2023. Paragraph 48.1.4 DAC Chip-specific Initialization states: "Enable VREF module...&amp;nbsp; DAC PTAT and ZTC current sources come from VREF module."&amp;nbsp; &amp;nbsp;What is the lowest power configuration of VREF that is needed for use of the DACs?&amp;nbsp; Does VREF buffering need to be enabled?&amp;nbsp; Using external reference for DAC reference select but DAC still apparently requires VREF for current source. Is there guidance regarding selection of PTAT vs ZTC, and what the tradeoffs are?&amp;nbsp; Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 15:27:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-VREF-dependency/m-p/2247498#M59010</guid>
      <dc:creator>TRCooper</dc:creator>
      <dc:date>2025-11-24T15:27:00Z</dc:date>
    </item>
    <item>
      <title>Re: DAC VREF dependency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-VREF-dependency/m-p/2249822#M59023</link>
      <description>&lt;P&gt;For minimum power, you can configure VREF in bandgap-only mode and disable unnecessary features. Buffering is not required if you are not using VREF_OUT as the DAC reference.&lt;BR /&gt;More details for VREF, please refer to the attached presentations on this post: &lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-on-DAC-current-sources-ZTC-PTAT/m-p/2159839" target="_blank"&gt;LPC5536: on DAC current sources (ZTC, PTAT)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 22:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-VREF-dependency/m-p/2249822#M59023</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-11-26T22:36:29Z</dc:date>
    </item>
  </channel>
</rss>