<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Max allowed function clock to MCAN module(s) in LPC5428 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2204935#M58990</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp;many thanks for your answer. I see from the SDK samples that 20 MHz is selected in all of them, but I was not able to find a number in either the DS or UM.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Nov 2025 06:49:59 GMT</pubDate>
    <dc:creator>carstengroen</dc:creator>
    <dc:date>2025-11-14T06:49:59Z</dc:date>
    <item>
      <title>Max allowed function clock to MCAN module(s) in LPC5428</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2200900#M58968</link>
      <description>&lt;P&gt;What is the maximum allowed clock to the MCAN module in the LPC54628 devices ?&lt;/P&gt;&lt;P&gt;I can't seem to locate the actual number in UM/DS, the samples from SDK shows often 220MHz/11 =&amp;gt; 20 MHz, but interested in knowing what the max allowed clock is.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Nov 2025 14:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2200900#M58968</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2025-11-07T14:40:26Z</dc:date>
    </item>
    <item>
      <title>Re: Max allowed function clock to MCAN module(s) in LPC5428</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2204701#M58989</link>
      <description>&lt;P&gt;In theory, the MCAN source clock supports higher frequency, it is limited by the mainclk.&lt;BR /&gt;MCAN functional clock for LPC546xx is 20 MHz, supports timing configurations for up to 5 Mbps data phase when using proper segment settings and prescalers. This limit is limited by the maximum supported CAN bit rate and protocol timings.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 13 Nov 2025 21:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2204701#M58989</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-11-13T21:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: Max allowed function clock to MCAN module(s) in LPC5428</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2204935#M58990</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp;many thanks for your answer. I see from the SDK samples that 20 MHz is selected in all of them, but I was not able to find a number in either the DS or UM.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Nov 2025 06:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-allowed-function-clock-to-MCAN-module-s-in-LPC5428/m-p/2204935#M58990</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2025-11-14T06:49:59Z</dc:date>
    </item>
  </channel>
</rss>