<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4088FET180 I2C1 pins - input impedance and current sinking when micro not powered</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2201068#M58969</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using an LPC4088FET180 micro on a single board computer (SBC) design. This board also incorporates an RTC chip. This chip uses a 3.0V coin cell for backup power when power is removed to the SBC. The I2C clock and data lines are pulled high through external 4.75k Ohm resistors.&lt;/P&gt;&lt;P&gt;I am trying to determine if there is a spec for the LPC4088FET180's I2C1 clock and data pins input impedance or ability to sink current, when power is removed from our single board computer (Vdd=0V). I think these pins should be high-Z when the LPC4088FET180 is not powered. I believe there are pull-up and/or pull-down resistors that can be present on the clock and data pins. So, I am not sure what the state of these pull-up or pull-down resistors would be on the I2C1 pins, when power is not applied to the micro (Vdd=0V). The information I can found in the datasheet related to the pull-ups or pull-downs, seems to be specific to Vdd being 3.3V. However, I am interested in knowing what the pull-up or pull-down values and states are when Vdd is 0V. I appreciate any help or information possible on this topic.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Nov 2025 21:32:40 GMT</pubDate>
    <dc:creator>longboard</dc:creator>
    <dc:date>2025-11-07T21:32:40Z</dc:date>
    <item>
      <title>LPC4088FET180 I2C1 pins - input impedance and current sinking when micro not powered</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2201068#M58969</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using an LPC4088FET180 micro on a single board computer (SBC) design. This board also incorporates an RTC chip. This chip uses a 3.0V coin cell for backup power when power is removed to the SBC. The I2C clock and data lines are pulled high through external 4.75k Ohm resistors.&lt;/P&gt;&lt;P&gt;I am trying to determine if there is a spec for the LPC4088FET180's I2C1 clock and data pins input impedance or ability to sink current, when power is removed from our single board computer (Vdd=0V). I think these pins should be high-Z when the LPC4088FET180 is not powered. I believe there are pull-up and/or pull-down resistors that can be present on the clock and data pins. So, I am not sure what the state of these pull-up or pull-down resistors would be on the I2C1 pins, when power is not applied to the micro (Vdd=0V). The information I can found in the datasheet related to the pull-ups or pull-downs, seems to be specific to Vdd being 3.3V. However, I am interested in knowing what the pull-up or pull-down values and states are when Vdd is 0V. I appreciate any help or information possible on this topic.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Nov 2025 21:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2201068#M58969</guid>
      <dc:creator>longboard</dc:creator>
      <dc:date>2025-11-07T21:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088FET180 I2C1 pins - input impedance and current sinking when micro not powered</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2201624#M58976</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256666"&gt;@longboard&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have checked the&amp;nbsp;LPC408x/7x data sheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1762760385826.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/364642i32DFAD82C622628F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1762760385826.png" alt="Harry_Zhang_0-1762760385826.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1762760385826.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;the LPC408x/7x family datasheet says the I²C pins are true open-drain and “when power is switched off, this pin connected to the I²C-bus is floating and does not disturb the I²C lines.” In other words, the pin driver itself goes high-Z when VDD = 0 V.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 10 Nov 2025 07:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2201624#M58976</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-11-10T07:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088FET180 I2C1 pins - input impedance and current sinking when micro not powered</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2202090#M58977</link>
      <description>&lt;P&gt;Hi Harry,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for pointing me to that information in the LPC408x/7x datasheet regarding the I2C bus pins state when Vdd=0V. I am glad to learn that the inputs are high-Z when Vdd=0V.&lt;/P&gt;&lt;P&gt;cheers,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
      <pubDate>Mon, 10 Nov 2025 19:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088FET180-I2C1-pins-input-impedance-and-current-sinking-when/m-p/2202090#M58977</guid>
      <dc:creator>longboard</dc:creator>
      <dc:date>2025-11-10T19:19:58Z</dc:date>
    </item>
  </channel>
</rss>