<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC 5V tolerant pins</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2196081#M58939</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249400"&gt;@tommino&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The distinction between pins and pads only matters if you are using the&amp;nbsp;HVQFN33 package of the LPC824. In general terms you can consider them equal.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 20:02:06 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2025-10-30T20:02:06Z</dc:date>
    <item>
      <title>LPC 5V tolerant pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195220#M58934</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am wondering if the LPC824 when powered at 3V3 has some pins that are 5V tolerant and can be used as digital input to get data with 0-5V logic.&lt;/P&gt;&lt;P&gt;Can you help me to find out this detail?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 15:29:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195220#M58934</guid>
      <dc:creator>tommino</dc:creator>
      <dc:date>2025-10-29T15:29:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 5V tolerant pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195279#M58935</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249400"&gt;@tommino&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM10800" target="_self"&gt;LPC82x User Manual&lt;/A&gt; states what pins are 5V tolerant on "Table 405. Pin description". Specifically, look at the footnotes of the 4th column in that table. In general, if the pin has a&amp;nbsp;[2],&amp;nbsp;[3],&amp;nbsp;[4],&amp;nbsp;[5] or&amp;nbsp;[8] footnote, it is 5V tolerant (see the footnotes for exceptions of each).&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 18:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195279#M58935</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-29T18:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 5V tolerant pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195600#M58937</link>
      <description>Hi Edwin,&lt;BR /&gt;&lt;BR /&gt;Thanks for the message. Could you please also tell me the difference between a "5V tolerant pin" and a "5V tolerant pad"?</description>
      <pubDate>Thu, 30 Oct 2025 07:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2195600#M58937</guid>
      <dc:creator>tommino</dc:creator>
      <dc:date>2025-10-30T07:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 5V tolerant pins</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2196081#M58939</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249400"&gt;@tommino&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The distinction between pins and pads only matters if you are using the&amp;nbsp;HVQFN33 package of the LPC824. In general terms you can consider them equal.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 20:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-5V-tolerant-pins/m-p/2196081#M58939</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-30T20:02:06Z</dc:date>
    </item>
  </channel>
</rss>