<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC11U24 zero length packets</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U24-zero-length-packets/m-p/523256#M5892</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by liaochengyi on Wed Apr 02 18:48:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also need know how to send zero length packets when data ending&amp;nbsp; used bulk in transfer in LPC11Uxx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If someone will answer the question?&amp;nbsp; NXP guys will help that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3Q&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chengyi&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:44:12 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:44:12Z</dc:date>
    <item>
      <title>LPC11U24 zero length packets</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U24-zero-length-packets/m-p/523255#M5891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcware_user on Tue Mar 04 07:18:34 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi there,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;we want to use a LPC11U24 mcu. The controller looks fine but i missed a detail. I have made good experience with&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the LPCUSBlib (running on LPC1833) and the hardware is working fine. For the LPC11U24 i want to know if it's&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;possible to generate a zero packet for an IN endpoint ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to transfer 128 bytes to the host but the buffer must be "closed" using a zero packet. I can call&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DcdDataTransfer() to prime the data for transmission. Either 128 bytes at all, or using two steps with 64 bytes each.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But can i call DcdDataTransfer() with length = 0 ?? Is the USB hardware generating a zero packet ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;lpcware_user&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U24-zero-length-packets/m-p/523255#M5891</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11U24 zero length packets</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U24-zero-length-packets/m-p/523256#M5892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by liaochengyi on Wed Apr 02 18:48:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also need know how to send zero length packets when data ending&amp;nbsp; used bulk in transfer in LPC11Uxx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If someone will answer the question?&amp;nbsp; NXP guys will help that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3Q&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chengyi&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U24-zero-length-packets/m-p/523256#M5892</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:44:12Z</dc:date>
    </item>
  </channel>
</rss>