<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1788 write external flash</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-write-external-flash/m-p/2191580#M58903</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;for my job I have to design a project based on LPC1788 where some data are received by UART and then must be written in memory.&lt;BR /&gt;Initially I wanted to use an external SPI EEPROM but because of data size (several Mbits) I need to use an external flash memory connected by EMC.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the past I have used EMC for SDRAM, never for Flash. How can I write a single buffer of data into external flash? I don't want to write low level read/write functions from external flash because it is complex and I wonder if there is a simple way&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Oct 2025 13:08:19 GMT</pubDate>
    <dc:creator>lorenzogalbiati</dc:creator>
    <dc:date>2025-10-23T13:08:19Z</dc:date>
    <item>
      <title>LPC1788 write external flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-write-external-flash/m-p/2191580#M58903</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;for my job I have to design a project based on LPC1788 where some data are received by UART and then must be written in memory.&lt;BR /&gt;Initially I wanted to use an external SPI EEPROM but because of data size (several Mbits) I need to use an external flash memory connected by EMC.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the past I have used EMC for SDRAM, never for Flash. How can I write a single buffer of data into external flash? I don't want to write low level read/write functions from external flash because it is complex and I wonder if there is a simple way&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Oct 2025 13:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-write-external-flash/m-p/2191580#M58903</guid>
      <dc:creator>lorenzogalbiati</dc:creator>
      <dc:date>2025-10-23T13:08:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 write external flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-write-external-flash/m-p/2192792#M58910</link>
      <description>&lt;P&gt;Flash are written on pages, unlike SDRAM. For examples, to configure the flash, I found these two post that may be helpful: &lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Spansion-EMC-NOR-Flash-on-LPC1788/m-p/517788" target="_blank"&gt;Spansion EMC NOR Flash on LPC1788 - NXP Community&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE/EMC-LPC1788-s29gl064-norFlash/m-p/530058" target="_blank"&gt;EMC + LPC1788 + s29gl064 norFlash - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 24 Oct 2025 22:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-write-external-flash/m-p/2192792#M58910</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-10-24T22:23:41Z</dc:date>
    </item>
  </channel>
</rss>