<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet Code using PHY DP83848CLPC Expresso IDE software for coding LPC2478 controller in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-using-PHY-DP83848CLPC-Expresso-IDE-software-for/m-p/2187163#M58865</link>
    <description>&lt;P&gt;&lt;STRONG&gt;Ethernet Code using PHY DP83848CLPC Expresso IDE software for coding LPC2478 controller&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am working on ethernet drive code LPC2478 controller connect to PHY DP83848C IC used for Ethernet communication of two LPC2478 controller using Ethernet cable RSOUT CONNECT TO SST39VF3202C RST# ALSO CONNECT TO RSTOUT LPC2478 here in code I used SRAM for EMAC address data tx and Rx I want code in LPCXPresso IDE my SRAM Memory Address is 0x7FE00000 (ETH_RAM_BASE) A configurable location in RAM used to&lt;BR /&gt;store the actual data (descriptors, buffers). but in LPCXpresso IDE vender file LPC24xx.h file only MAC_RXDESCADDR (0xFFE00204) Fixed hardware address used to tell the how can solve this issue in LPCXPresso IDE&amp;nbsp;&lt;BR /&gt;EMAC DMA where your memory&lt;BR /&gt;structures start.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Oct 2025 05:25:33 GMT</pubDate>
    <dc:creator>VijayaJangam1</dc:creator>
    <dc:date>2025-10-16T05:25:33Z</dc:date>
    <item>
      <title>Ethernet Code using PHY DP83848CLPC Expresso IDE software for coding LPC2478 controller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-using-PHY-DP83848CLPC-Expresso-IDE-software-for/m-p/2187163#M58865</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Ethernet Code using PHY DP83848CLPC Expresso IDE software for coding LPC2478 controller&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am working on ethernet drive code LPC2478 controller connect to PHY DP83848C IC used for Ethernet communication of two LPC2478 controller using Ethernet cable RSOUT CONNECT TO SST39VF3202C RST# ALSO CONNECT TO RSTOUT LPC2478 here in code I used SRAM for EMAC address data tx and Rx I want code in LPCXPresso IDE my SRAM Memory Address is 0x7FE00000 (ETH_RAM_BASE) A configurable location in RAM used to&lt;BR /&gt;store the actual data (descriptors, buffers). but in LPCXpresso IDE vender file LPC24xx.h file only MAC_RXDESCADDR (0xFFE00204) Fixed hardware address used to tell the how can solve this issue in LPCXPresso IDE&amp;nbsp;&lt;BR /&gt;EMAC DMA where your memory&lt;BR /&gt;structures start.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 05:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-using-PHY-DP83848CLPC-Expresso-IDE-software-for/m-p/2187163#M58865</guid>
      <dc:creator>VijayaJangam1</dc:creator>
      <dc:date>2025-10-16T05:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Code using PHY DP83848CLPC Expresso IDE software for coding LPC2478 controller</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-using-PHY-DP83848CLPC-Expresso-IDE-software-for/m-p/2189905#M58892</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253577" target="_blank"&gt;@VijayaJangam1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It seems this question is the same as the one posted at&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A class="fui-Link ___w5et180 f2hkw1w f3rmtva f1ewtqcl fyind8e f1k6fduh f1w7gpdv f1mo0ibp fjoy568 ff5ikls f1s184ao f1mk8lai fnbmjn9 f1o700av f13mvf36 f1cmlufx f9n3di6 f1ids18y f1tx3yz7 f1deo86v f1eh06m1 f1iescvh fhgqx19 f1olyrje f1p93eir f1nev41a" tabindex="0" href="https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-For-LPC2478-controller-using-LPC24xx-h-file-on/m-p/2186537" target="_blank" rel="noopener" data-tabster="{&amp;quot;restorer&amp;quot;:{&amp;quot;type&amp;quot;:1}}"&gt;this link&lt;/A&gt;. My colleague will reply to you in that thread. No need create so many tickets.&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 10:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-Code-using-PHY-DP83848CLPC-Expresso-IDE-software-for/m-p/2189905#M58892</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-10-21T10:36:29Z</dc:date>
    </item>
  </channel>
</rss>