<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC546XX CTIMER configuration question</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-CTIMER-configuration-question/m-p/2176873#M58822</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254989"&gt;@abdel12312&lt;/a&gt;, sorry for the late reply.&lt;BR /&gt;Yes, you can configure a channel in Input Capture/Match mode and utilize the match register simultaneously. However, the SDK does not provide an example demonstrating both functionalities together. As a reference, you can modify the example named lpcxpresso54628_ctimer_match_interrupt_example, which already includes the match functionality. This &lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/CTimer-capture-examples-for-LPC54608/m-p/819863" target="_self"&gt;thread&lt;/A&gt; may also help guide your implementation.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Sep 2025 23:40:28 GMT</pubDate>
    <dc:creator>Habib_MS</dc:creator>
    <dc:date>2025-09-26T23:40:28Z</dc:date>
    <item>
      <title>LPC546XX CTIMER configuration question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-CTIMER-configuration-question/m-p/2172144#M58777</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I'm working with an LPC546xx and need to know if a single CTIMER can simultaneously:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use channels 0 and 1 for input capture&lt;/LI&gt;&lt;LI&gt;Use a match register (MR0) for interrupt generation on counter overflow without affecting any pins&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;My current setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;CTIMER1 channels 0-1: Input capture&lt;/LI&gt;&lt;LI&gt;CTIMER1 channels 2-3: Timeout interrupts&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I need to add timer overflow detection using a match register on the same timer. My though was to use Channels 0 or 1 MRs to be able to count number of overflows.&lt;/P&gt;&lt;P&gt;Since MCR (match control), CCR (capture control), and EMR (pin output) are separate registers, I believe they can be configured independently.&lt;/P&gt;&lt;P&gt;Can someone from NXP confirm if using match interrupts alongside input capture is supported?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 16:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-CTIMER-configuration-question/m-p/2172144#M58777</guid>
      <dc:creator>abdel12312</dc:creator>
      <dc:date>2025-09-18T16:05:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546XX CTIMER configuration question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-CTIMER-configuration-question/m-p/2176873#M58822</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254989"&gt;@abdel12312&lt;/a&gt;, sorry for the late reply.&lt;BR /&gt;Yes, you can configure a channel in Input Capture/Match mode and utilize the match register simultaneously. However, the SDK does not provide an example demonstrating both functionalities together. As a reference, you can modify the example named lpcxpresso54628_ctimer_match_interrupt_example, which already includes the match functionality. This &lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/CTimer-capture-examples-for-LPC54608/m-p/819863" target="_self"&gt;thread&lt;/A&gt; may also help guide your implementation.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 23:40:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-CTIMER-configuration-question/m-p/2176873#M58822</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-09-26T23:40:28Z</dc:date>
    </item>
  </channel>
</rss>