<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RBS bit not setting in LPC1768 CAN driver in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/RBS-bit-not-setting-in-LPC1768-CAN-driver/m-p/2174803#M58800</link>
    <description>&lt;P&gt;The CAN controller is configured correctly — bit timing is set, it enters normal mode, and incoming frames are visible . Registers &lt;STRONG&gt;CANxRFS, CANxRID, and CANxRDA&lt;/STRONG&gt;&amp;nbsp;are updated correctly when a frame is received. I am implementing an interrupt-driven CAN driver on LPC1768 with a baud rate of 500 kbps.&lt;/P&gt;&lt;P&gt;However, the &lt;STRONG&gt;RBS (Receive Buffer Status) bit does not get set in either CANxSR or CANxGSR&lt;/STRONG&gt;, even though a complete CAN frame is received. I am not setting the RRB bit in CANxCMR to release the receive buffer, so the RBS bit should remain set until the buffer is released.&lt;/P&gt;&lt;P&gt;Could you please explain why the RBS bit might not set, or if there are any known issues with LPC1768 CAN in this setup?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
    <pubDate>Wed, 24 Sep 2025 06:41:46 GMT</pubDate>
    <dc:creator>Nisarga</dc:creator>
    <dc:date>2025-09-24T06:41:46Z</dc:date>
    <item>
      <title>RBS bit not setting in LPC1768 CAN driver</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/RBS-bit-not-setting-in-LPC1768-CAN-driver/m-p/2174803#M58800</link>
      <description>&lt;P&gt;The CAN controller is configured correctly — bit timing is set, it enters normal mode, and incoming frames are visible . Registers &lt;STRONG&gt;CANxRFS, CANxRID, and CANxRDA&lt;/STRONG&gt;&amp;nbsp;are updated correctly when a frame is received. I am implementing an interrupt-driven CAN driver on LPC1768 with a baud rate of 500 kbps.&lt;/P&gt;&lt;P&gt;However, the &lt;STRONG&gt;RBS (Receive Buffer Status) bit does not get set in either CANxSR or CANxGSR&lt;/STRONG&gt;, even though a complete CAN frame is received. I am not setting the RRB bit in CANxCMR to release the receive buffer, so the RBS bit should remain set until the buffer is released.&lt;/P&gt;&lt;P&gt;Could you please explain why the RBS bit might not set, or if there are any known issues with LPC1768 CAN in this setup?&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 06:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/RBS-bit-not-setting-in-LPC1768-CAN-driver/m-p/2174803#M58800</guid>
      <dc:creator>Nisarga</dc:creator>
      <dc:date>2025-09-24T06:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: RBS bit not setting in LPC1768 CAN driver</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/RBS-bit-not-setting-in-LPC1768-CAN-driver/m-p/2176507#M58815</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247852"&gt;@Nisarga&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on your description,&lt;/P&gt;
&lt;P&gt;I think you can check&amp;nbsp;AFMR register.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1758878166234.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358712i719B65820C9B1EAD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1758878166234.png" alt="Harry_Zhang_0-1758878166234.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1758878166234.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I think If acceptance filtering is bypassed, messages go directly into the Receive Registers (CANxRFS/RID/RDA/RDB) without updating RBS.&lt;/P&gt;
&lt;P&gt;You can check it.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 09:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/RBS-bit-not-setting-in-LPC1768-CAN-driver/m-p/2176507#M58815</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-09-26T09:22:24Z</dc:date>
    </item>
  </channel>
</rss>