<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCUXpresso doesn't connect to target in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-doesn-t-connect-to-target/m-p/2157523#M58690</link>
    <description>&lt;P&gt;Ladies and Gentlemen,&lt;/P&gt;&lt;P&gt;I've got MCUXpresso 25.6 [Build 136] recently installed on my Linux Mint 22.1 Cinnamon machine.&lt;/P&gt;&lt;P&gt;I'm trying to get familiar with the development system and uC programming, too.&lt;/P&gt;&lt;P&gt;I connected an LPC11U37H LPCXpresso board (it is original from NXP, but was in the drawer for a few years). Also, I wrote a very primitive program, just trying to configure the microcontroller. (clocks, peripherals, etc)&lt;/P&gt;&lt;P&gt;When I try to debug my code, it builds without failure but MCUXpresso cannot connect to the debugger board:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_0-1756118582696.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353929iF356BDCF110EBC9E/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_0-1756118582696.png" title="jeanvaljean_0-1756118582696.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, if I close MCUXpresso and try to use LinkFlash 25.6.131 - it is automatically installed together with MCUXpresso - then I see, this SW connected to the probe with no issue:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_1-1756118823825.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353930iC576A3C226F69A0D/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_1-1756118823825.png" title="jeanvaljean_1-1756118823825.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My own code doesn't work yet - no surprise - but I could only debug it inside MCUXpresso.&lt;/P&gt;&lt;P&gt;Here's the output of LSUSB:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_2-1756118935837.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353931i035BD59B61CCD980/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_2-1756118935837.png" title="jeanvaljean_2-1756118935837.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have read this post from Helmut, but it didn't help:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/Could-not-connect-to-target/m-p/1297670#M7068" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/Could-not-connect-to-target/m-p/1297670#M7068&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Please give me advice, what shall I set to use this board?&lt;/P&gt;</description>
    <pubDate>Mon, 25 Aug 2025 10:55:24 GMT</pubDate>
    <dc:creator>jeanvaljean</dc:creator>
    <dc:date>2025-08-25T10:55:24Z</dc:date>
    <item>
      <title>MCUXpresso doesn't connect to target</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-doesn-t-connect-to-target/m-p/2157523#M58690</link>
      <description>&lt;P&gt;Ladies and Gentlemen,&lt;/P&gt;&lt;P&gt;I've got MCUXpresso 25.6 [Build 136] recently installed on my Linux Mint 22.1 Cinnamon machine.&lt;/P&gt;&lt;P&gt;I'm trying to get familiar with the development system and uC programming, too.&lt;/P&gt;&lt;P&gt;I connected an LPC11U37H LPCXpresso board (it is original from NXP, but was in the drawer for a few years). Also, I wrote a very primitive program, just trying to configure the microcontroller. (clocks, peripherals, etc)&lt;/P&gt;&lt;P&gt;When I try to debug my code, it builds without failure but MCUXpresso cannot connect to the debugger board:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_0-1756118582696.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353929iF356BDCF110EBC9E/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_0-1756118582696.png" title="jeanvaljean_0-1756118582696.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, if I close MCUXpresso and try to use LinkFlash 25.6.131 - it is automatically installed together with MCUXpresso - then I see, this SW connected to the probe with no issue:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_1-1756118823825.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353930iC576A3C226F69A0D/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_1-1756118823825.png" title="jeanvaljean_1-1756118823825.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My own code doesn't work yet - no surprise - but I could only debug it inside MCUXpresso.&lt;/P&gt;&lt;P&gt;Here's the output of LSUSB:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jeanvaljean_2-1756118935837.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353931i035BD59B61CCD980/image-size/medium?v=v2&amp;amp;px=400" alt="jeanvaljean_2-1756118935837.png" title="jeanvaljean_2-1756118935837.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have read this post from Helmut, but it didn't help:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/Could-not-connect-to-target/m-p/1297670#M7068" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/Could-not-connect-to-target/m-p/1297670#M7068&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Please give me advice, what shall I set to use this board?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 10:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-doesn-t-connect-to-target/m-p/2157523#M58690</guid>
      <dc:creator>jeanvaljean</dc:creator>
      <dc:date>2025-08-25T10:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso doesn't connect to target</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-doesn-t-connect-to-target/m-p/2157609#M58691</link>
      <description>&lt;P&gt;Found a solution - after a few days of try-and-error:&lt;BR /&gt;Left side, in the project explorer window, right-click on the project name.&lt;BR /&gt;In the pop-up&amp;nbsp; menu, select Debug As -&amp;gt; 2 MCUXpresso IDE Link Server (inc. CMSIS-DAP) probes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And, voila!&amp;nbsp; It works.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 14:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUXpresso-doesn-t-connect-to-target/m-p/2157609#M58691</guid>
      <dc:creator>jeanvaljean</dc:creator>
      <dc:date>2025-08-25T14:01:10Z</dc:date>
    </item>
  </channel>
</rss>