<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC8N04 I2C not working</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8N04-I2C-not-working/m-p/2148974#M58622</link>
    <description>&lt;P&gt;I have the OM40002 Dev board.&lt;/P&gt;&lt;P&gt;The problem I see is that, when attaching a logic probe to SDA and SCL, I just see both lines as perpetually high. (I am using the maximum sample rate on my probe of 48MHz).&lt;/P&gt;&lt;P&gt;Here is my code:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#include "LPC8N04.h"

#define I2C_CLOCK (1u &amp;lt;&amp;lt; 5)

int main(void) {
  // Init pins
  IOCON-&amp;gt;PIO[0][4] = 1u; // SCL
  IOCON-&amp;gt;PIO[0][5] = 1u; // SDA

  // Init clocks
  SYSCON-&amp;gt;SYSCLKCTRL &amp;amp;= ~0b1110u; // SYSCLKDIV = 0 =&amp;gt; 8MHz
  SYSCON-&amp;gt;SYSCLKUEN &amp;amp;= ~1u;       // Update system clock source
  SYSCON-&amp;gt;SYSCLKUEN |= 1u;
  SYSCON-&amp;gt;WDTCLKDIV = 1;
  SYSCON-&amp;gt;SYSAHBCLKCTRL |= I2C_CLOCK;

  SYSCON-&amp;gt;PRESETCTRL |= 0b10;
  I2C0-&amp;gt;CONCLR = 0b01101100;
  I2C0-&amp;gt;SCLH = 80; // 8 MHz / 80 = 100 kHz
  I2C0-&amp;gt;SCLL = 80;
  I2C0-&amp;gt;CONSET = 0b01000000; // I2EN

  I2C0-&amp;gt;CONSET = I2C0_CONSET_STA_MASK;          // START
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;
  I2C0-&amp;gt;DAT = 0xAE;                             // Send slave addr
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;
  I2C0-&amp;gt;CONCLR |= (1 &amp;lt;&amp;lt; 3);
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;

  while (1) {
  }
}&lt;/LI-CODE&gt;&lt;P&gt;Debugging shows that the program spins forever on the second to last while loop (just after CONCLR)&lt;/P&gt;&lt;P&gt;I have split the board in two and wired the 6 debug pins between the two halves since I thought that the connection to the LED array could cause problems.&lt;/P&gt;&lt;P&gt;I have wired P4-1 (PIO0_4/SCL) and P4-3 (PIO0_5/SDA) to P4-5 (VCC) via pull up resistors.&lt;/P&gt;&lt;P&gt;I have tried pull up resistors from 1k to 100k and get the same result.&lt;/P&gt;&lt;P&gt;I have tried running both with and without a slave device connected.&lt;/P&gt;&lt;P&gt;Nothing I have tried has caused any output on SDA or SCL.&lt;/P&gt;&lt;P&gt;I have tried multiple methods of compiling and flashing the code, including just creating a new project in mcuexpresso with default options and just changing the main method to the above.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Aug 2025 07:28:47 GMT</pubDate>
    <dc:creator>TheOrangeTeaFrog</dc:creator>
    <dc:date>2025-08-08T07:28:47Z</dc:date>
    <item>
      <title>LPC8N04 I2C not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8N04-I2C-not-working/m-p/2148974#M58622</link>
      <description>&lt;P&gt;I have the OM40002 Dev board.&lt;/P&gt;&lt;P&gt;The problem I see is that, when attaching a logic probe to SDA and SCL, I just see both lines as perpetually high. (I am using the maximum sample rate on my probe of 48MHz).&lt;/P&gt;&lt;P&gt;Here is my code:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#include "LPC8N04.h"

#define I2C_CLOCK (1u &amp;lt;&amp;lt; 5)

int main(void) {
  // Init pins
  IOCON-&amp;gt;PIO[0][4] = 1u; // SCL
  IOCON-&amp;gt;PIO[0][5] = 1u; // SDA

  // Init clocks
  SYSCON-&amp;gt;SYSCLKCTRL &amp;amp;= ~0b1110u; // SYSCLKDIV = 0 =&amp;gt; 8MHz
  SYSCON-&amp;gt;SYSCLKUEN &amp;amp;= ~1u;       // Update system clock source
  SYSCON-&amp;gt;SYSCLKUEN |= 1u;
  SYSCON-&amp;gt;WDTCLKDIV = 1;
  SYSCON-&amp;gt;SYSAHBCLKCTRL |= I2C_CLOCK;

  SYSCON-&amp;gt;PRESETCTRL |= 0b10;
  I2C0-&amp;gt;CONCLR = 0b01101100;
  I2C0-&amp;gt;SCLH = 80; // 8 MHz / 80 = 100 kHz
  I2C0-&amp;gt;SCLL = 80;
  I2C0-&amp;gt;CONSET = 0b01000000; // I2EN

  I2C0-&amp;gt;CONSET = I2C0_CONSET_STA_MASK;          // START
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;
  I2C0-&amp;gt;DAT = 0xAE;                             // Send slave addr
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;
  I2C0-&amp;gt;CONCLR |= (1 &amp;lt;&amp;lt; 3);
  while (!(I2C0-&amp;gt;CONSET &amp;amp; I2C0_CONSET_SI_MASK)) // Wait
    ;

  while (1) {
  }
}&lt;/LI-CODE&gt;&lt;P&gt;Debugging shows that the program spins forever on the second to last while loop (just after CONCLR)&lt;/P&gt;&lt;P&gt;I have split the board in two and wired the 6 debug pins between the two halves since I thought that the connection to the LED array could cause problems.&lt;/P&gt;&lt;P&gt;I have wired P4-1 (PIO0_4/SCL) and P4-3 (PIO0_5/SDA) to P4-5 (VCC) via pull up resistors.&lt;/P&gt;&lt;P&gt;I have tried pull up resistors from 1k to 100k and get the same result.&lt;/P&gt;&lt;P&gt;I have tried running both with and without a slave device connected.&lt;/P&gt;&lt;P&gt;Nothing I have tried has caused any output on SDA or SCL.&lt;/P&gt;&lt;P&gt;I have tried multiple methods of compiling and flashing the code, including just creating a new project in mcuexpresso with default options and just changing the main method to the above.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 07:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8N04-I2C-not-working/m-p/2148974#M58622</guid>
      <dc:creator>TheOrangeTeaFrog</dc:creator>
      <dc:date>2025-08-08T07:28:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPC8N04 I2C not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8N04-I2C-not-working/m-p/2149148#M58623</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250837"&gt;@TheOrangeTeaFrog&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-JOTKXA paragraph-element br-paragraph-space"&gt;Thanks for your question.&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-JOTKXA paragraph-element br-paragraph-space"&gt;I recommend that you first run the I2C demo included in the SDK for your board. Confirm that it works properly, which will help verify there are no issues with your board. Then, make modifications to the demo based on your specific requirements.&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1754649011923.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351568i7492C19273BCC4FB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1754649011923.png" alt="Alice_Yang_0-1754649011923.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1754649011923.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-JOTKXA paragraph-element br-paragraph-space"&gt;Please let me know if you have any further questions.&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-JOTKXA paragraph-element br-paragraph-space"&gt;Thank you.&lt;/DIV&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 10:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC8N04-I2C-not-working/m-p/2149148#M58623</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-08-08T10:30:23Z</dc:date>
    </item>
  </channel>
</rss>