<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC5536 MCAN RF0F Interrupt</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2140365#M58546</link>
    <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;Thank you for your answer.&lt;BR /&gt;It is all fine with the IE register. I was just stating that the IE:RF0FE (it is the bit number 2 and not the bit number 3) was not being set and the and the IR:RF0F was being triggered. If it is an hardware thing, it is all right then.&lt;BR /&gt;It is just a little bit annoying to have a kStatus_MCAN_TxIdle and a kStatus_MCAN_UnHandled with result set to kMCAN_RxFifo0FullFlag for every received message.&lt;BR /&gt;&lt;BR /&gt;</description>
    <pubDate>Thu, 24 Jul 2025 20:28:38 GMT</pubDate>
    <dc:creator>microcris</dc:creator>
    <dc:date>2025-07-24T20:28:38Z</dc:date>
    <item>
      <title>LPC5536 MCAN RF0F Interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2127427#M58452</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Why am I getting this interrupt (IR:RF0F) if the IE:RF0FE is set to 0?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to figure this out by monitoring the IE register and it is changing from&amp;nbsp;0x3800000 to&amp;nbsp;0x3800001, the bit number 3 is not being set at anytime.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Cristiano Rodrigues&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 17:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2127427#M58452</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2025-07-02T17:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5536 MCAN RF0F Interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2128923#M58461</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/141639"&gt;@microcris&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks for your question. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The flag (IR:RF0F) is automatically set by the hardware and has no relation to the interrupt enable register IE:RF0FE. The IE register notifies the CPU to execute the interrupt handler. Regarding the change of IE bit 0 from 0 to 1, please debug the code to check where this bit is being modified. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 02:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2128923#M58461</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-07-07T02:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5536 MCAN RF0F Interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2140365#M58546</link>
      <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;Thank you for your answer.&lt;BR /&gt;It is all fine with the IE register. I was just stating that the IE:RF0FE (it is the bit number 2 and not the bit number 3) was not being set and the and the IR:RF0F was being triggered. If it is an hardware thing, it is all right then.&lt;BR /&gt;It is just a little bit annoying to have a kStatus_MCAN_TxIdle and a kStatus_MCAN_UnHandled with result set to kMCAN_RxFifo0FullFlag for every received message.&lt;BR /&gt;&lt;BR /&gt;</description>
      <pubDate>Thu, 24 Jul 2025 20:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2140365#M58546</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2025-07-24T20:28:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5536 MCAN RF0F Interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2141349#M58559</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/141639"&gt;@microcris&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The flag of kMCAN_RxFifo0FullFlag is to avoid Rx FIFO overflow.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jul 2025 03:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-MCAN-RF0F-Interrupt/m-p/2141349#M58559</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-07-28T03:17:14Z</dc:date>
    </item>
  </channel>
</rss>