<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPCXPRESSO LPC2103 ISP programmig</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXPRESSO-LPC2103-ISP-programmig/m-p/2137606#M58522</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241207"&gt;@oykr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;After building the project, a Debug folder should be created. Inside it, you will find a .axf file, which can be used to generate the binary for the project.&lt;/P&gt;
&lt;P&gt;This binary can then be used to program the MCU.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
    <pubDate>Mon, 21 Jul 2025 17:18:00 GMT</pubDate>
    <dc:creator>Pablo_Ramos</dc:creator>
    <dc:date>2025-07-21T17:18:00Z</dc:date>
    <item>
      <title>LPCXPRESSO LPC2103 ISP programmig</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXPRESSO-LPC2103-ISP-programmig/m-p/2137559#M58521</link>
      <description>&lt;P&gt;Hi. I have written a code small code proejct for LPC2103 with LPCXPRESSO. I want to program it ISP over UART0 interface. But which output file in LPCEXPRESSO do I need to UUENCODE and then program.?&lt;/P&gt;&lt;P&gt;kr&lt;/P&gt;&lt;P&gt;Øystein&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 15:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXPRESSO-LPC2103-ISP-programmig/m-p/2137559#M58521</guid>
      <dc:creator>oykr</dc:creator>
      <dc:date>2025-07-21T15:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXPRESSO LPC2103 ISP programmig</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXPRESSO-LPC2103-ISP-programmig/m-p/2137606#M58522</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241207"&gt;@oykr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;After building the project, a Debug folder should be created. Inside it, you will find a .axf file, which can be used to generate the binary for the project.&lt;/P&gt;
&lt;P&gt;This binary can then be used to program the MCU.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 17:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXPRESSO-LPC2103-ISP-programmig/m-p/2137606#M58522</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-07-21T17:18:00Z</dc:date>
    </item>
  </channel>
</rss>