<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC81x default state of GPIO</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2110783#M58311</link>
    <description>Thanks a lot.&lt;BR /&gt;We have around 200us~300us improvement with this solution. This should be enough to solve our problem during start-up.&lt;BR /&gt;</description>
    <pubDate>Thu, 05 Jun 2025 01:53:35 GMT</pubDate>
    <dc:creator>Sid_Zhou</dc:creator>
    <dc:date>2025-06-05T01:53:35Z</dc:date>
    <item>
      <title>LPC81x default state of GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2109136#M58292</link>
      <description>&lt;P&gt;We are using&amp;nbsp;LPC812M101JDH20 on one of our products. The datasheet specified the default state of GPIO(PIO0_16) is "Input with pull-up."&lt;/P&gt;&lt;P&gt;Somehow, in our application, we need this PIO0_16 to be open drain at the very early start-up stage. I am wondering if this default state can be modified somewhere within "startup_LPC8xx.s"&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 05:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2109136#M58292</guid>
      <dc:creator>Sid_Zhou</dc:creator>
      <dc:date>2025-06-03T05:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC81x default state of GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2110118#M58309</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159490"&gt;@Sid_Zhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can add related function in SystemInit.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Enable clock to IOCON block.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Configure PIO0_16 as open-drain output.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1749019316518.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341302i59BB0E4B57F1A599/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1749019316518.png" alt="Harry_Zhang_0-1749019316518.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Harry_Zhang_0-1749019316518.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 06:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2110118#M58309</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-06-04T06:43:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC81x default state of GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2110783#M58311</link>
      <description>Thanks a lot.&lt;BR /&gt;We have around 200us~300us improvement with this solution. This should be enough to solve our problem during start-up.&lt;BR /&gt;</description>
      <pubDate>Thu, 05 Jun 2025 01:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC81x-default-state-of-GPIO/m-p/2110783#M58311</guid>
      <dc:creator>Sid_Zhou</dc:creator>
      <dc:date>2025-06-05T01:53:35Z</dc:date>
    </item>
  </channel>
</rss>