<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピック12MHz FRO frequency change</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/12MHz-FRO-frequency-change/m-p/2107025#M58264</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LPC54608J512BD208 microcontroller in our product with 2 UART (FLEXCOMM2 and FLEXCOMM4) sourced from the 12MHz internal FRO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We saw that, from time to time, the baud rate of the UART changed to a lower value (it could take several days) and we confirmed (using a pin to output the 12MHz internal FRO) that the reason is frequency of the 12MHz FRO changed more or less 5% to a lower value.&lt;/P&gt;&lt;P&gt;I saw in this forum a similar issue:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605-fro-hf-drift-lower-than-48MHz-after-IEC-61000-4-3-EMC/td-p/1178745" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605-fro-hf-drift-lower-than-48MHz-after-IEC-61000-4-3-EMC/td-p/1178745&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Do you know why frequency is changing more than 1% indicated at datasheet?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 29 May 2025 09:03:34 GMT</pubDate>
    <dc:creator>F_Vaquero</dc:creator>
    <dc:date>2025-05-29T09:03:34Z</dc:date>
    <item>
      <title>12MHz FRO frequency change</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/12MHz-FRO-frequency-change/m-p/2107025#M58264</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using the LPC54608J512BD208 microcontroller in our product with 2 UART (FLEXCOMM2 and FLEXCOMM4) sourced from the 12MHz internal FRO.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We saw that, from time to time, the baud rate of the UART changed to a lower value (it could take several days) and we confirmed (using a pin to output the 12MHz internal FRO) that the reason is frequency of the 12MHz FRO changed more or less 5% to a lower value.&lt;/P&gt;&lt;P&gt;I saw in this forum a similar issue:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605-fro-hf-drift-lower-than-48MHz-after-IEC-61000-4-3-EMC/td-p/1178745" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/LPC54605-fro-hf-drift-lower-than-48MHz-after-IEC-61000-4-3-EMC/td-p/1178745&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Do you know why frequency is changing more than 1% indicated at datasheet?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 09:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/12MHz-FRO-frequency-change/m-p/2107025#M58264</guid>
      <dc:creator>F_Vaquero</dc:creator>
      <dc:date>2025-05-29T09:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: 12MHz FRO frequency change</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/12MHz-FRO-frequency-change/m-p/2107855#M58273</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/177653"&gt;@F_Vaquero&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;According the&amp;nbsp;LPC546xx Data Sheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1748593474252.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/340658i03E75CCFEB3D22AB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1748593474252.png" alt="Harry_Zhang_0-1748593474252.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The 12 MHz FRO (Free Running Oscillator) on the LPC54608J512 should typically stay within ±1% frequency accuracy across operating conditions, as stated in the datasheet.&lt;/P&gt;
&lt;P&gt;A drift of 5% is unusual and exceeds the expected spec. Since you're observing the FRO output changing after long durations (several days) and your UART baud rate is affected, this may indicate a hardware or environmental sensitivity issue.&lt;/P&gt;
&lt;P&gt;Your FRO drift issue likely results from EMC-induced trim corruption.&lt;/P&gt;
&lt;P&gt;So i think&amp;nbsp;the most robust solution is to switch to a crystal oscillator for clocking, especially for timing-critical subsystems like UART.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 08:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/12MHz-FRO-frequency-change/m-p/2107855#M58273</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-05-30T08:27:27Z</dc:date>
    </item>
  </channel>
</rss>