<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Connecting 64Mbits SDRAM to LPC54607 208pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connecting-64Mbits-SDRAM-to-LPC54607-208pin/m-p/2105560#M58243</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249462"&gt;@Lex2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you using lpcxpresso54608_emc_sdram as base for the setup of an external SDRAM? If not, I highly recommend you download the SDK example and use it as template in order to properly communicate with your SDRAM.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Tue, 27 May 2025 21:27:06 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2025-05-27T21:27:06Z</dc:date>
    <item>
      <title>Connecting 64Mbits SDRAM to LPC54607 208pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connecting-64Mbits-SDRAM-to-LPC54607-208pin/m-p/2101293#M58205</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I want to connect LPC54607 with&amp;nbsp;W9864G6KH-5(64Mbits,&amp;nbsp;4 banks x 16 bits).&amp;nbsp;&lt;BR /&gt;My schematic is attached.&amp;nbsp;&lt;BR /&gt;I have already created PCB board and placed the MCU and the SDRAM.&lt;BR /&gt;I tested memory-write-read the SDRAM.&lt;BR /&gt;Test is passed in first bank(0xa00000000 ~ 0xa0200000).&lt;BR /&gt;But, there are garbage data all in second bank(0xa0200000~0xa0400000) test.&lt;BR /&gt;I probed A13 address line in testing second bank. I can not see any movements. But A14 pin has something moving. I can not understand why MCU sends some signal to A14.&lt;BR /&gt;My setting values are&lt;BR /&gt;#define SDRAM_MODEREG_VALUE (0x33u)&lt;BR /&gt;#define SDRAM_DEV_MEMORYMAP (0x25u) /* 64Mbits (4M*16, 4banks, 12 rows, 8 columns)*/&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;DYNAMICCONFIG[0] is&amp;nbsp; 0x00081280(I captured this value by SWD).&lt;/P&gt;&lt;P&gt;I guess MCU believed that bank selection[0:1] are connected A13,A14. But, It must be A12,A13.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please tell me anything my mistake or misunderstanding.&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 07:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Connecting-64Mbits-SDRAM-to-LPC54607-208pin/m-p/2101293#M58205</guid>
      <dc:creator>Lex2</dc:creator>
      <dc:date>2025-05-21T07:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting 64Mbits SDRAM to LPC54607 208pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Connecting-64Mbits-SDRAM-to-LPC54607-208pin/m-p/2105560#M58243</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249462"&gt;@Lex2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you using lpcxpresso54608_emc_sdram as base for the setup of an external SDRAM? If not, I highly recommend you download the SDK example and use it as template in order to properly communicate with your SDRAM.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 27 May 2025 21:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Connecting-64Mbits-SDRAM-to-LPC54607-208pin/m-p/2105560#M58243</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-05-27T21:27:06Z</dc:date>
    </item>
  </channel>
</rss>