<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S28 read SYST_CVR register data is always 0 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-read-SYST-CVR-register-data-is-always-0/m-p/2089687#M58148</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245163"&gt;@MHY_0878&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The SDK (version 25.03) includes an example named "led_blinky_lpc" that demonstrates the use of the SysTick timer. I highly recommend reviewing this example to understand its functionality, particularly the "SysTick_Config" function where the SysTick timer is configured.&lt;/P&gt;
&lt;P&gt;For additional information, please refer to Chapter 29, titled "System Tick Timer," in the Reference Manual (RM).&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
    <pubDate>Tue, 29 Apr 2025 22:31:12 GMT</pubDate>
    <dc:creator>Habib_MS</dc:creator>
    <dc:date>2025-04-29T22:31:12Z</dc:date>
    <item>
      <title>LPC55S28 read SYST_CVR register data is always 0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-read-SYST-CVR-register-data-is-always-0/m-p/2087149#M58135</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello everyone, I read SYST_CVR register in LPC5528 microcontroller all the time to 0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;void Test_sys_timer(void)&lt;BR /&gt;{&lt;BR /&gt;uint32_t time1,time2 = 0;&lt;BR /&gt;&lt;BR /&gt;SYST_CVR = 0xffffffff;&lt;BR /&gt;SYST_CSR = 0x5;&lt;BR /&gt;time1 = SYST_CVR;&lt;BR /&gt;delay();//os_msleep(1);&lt;BR /&gt;time2 = SYST_CVR;&lt;BR /&gt;&lt;BR /&gt;//SYST_CSR = 0x00;&lt;BR /&gt;&lt;BR /&gt;usb_echo("data = %u\r\n",time1-time2);&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I don't know why, please help me, or could you please recommend me a clock configuration for SYST_CVR, I don't know much about it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings from MHY.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Apr 2025 07:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-read-SYST-CVR-register-data-is-always-0/m-p/2087149#M58135</guid>
      <dc:creator>MHY_0878</dc:creator>
      <dc:date>2025-04-25T07:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28 read SYST_CVR register data is always 0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-read-SYST-CVR-register-data-is-always-0/m-p/2089687#M58148</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245163"&gt;@MHY_0878&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The SDK (version 25.03) includes an example named "led_blinky_lpc" that demonstrates the use of the SysTick timer. I highly recommend reviewing this example to understand its functionality, particularly the "SysTick_Config" function where the SysTick timer is configured.&lt;/P&gt;
&lt;P&gt;For additional information, please refer to Chapter 29, titled "System Tick Timer," in the Reference Manual (RM).&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 22:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-read-SYST-CVR-register-data-is-always-0/m-p/2089687#M58148</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-04-29T22:31:12Z</dc:date>
    </item>
  </channel>
</rss>