<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Max throughput of LPC546xx MCU HS High Speed USB in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-throughput-of-LPC546xx-MCU-HS-High-Speed-USB/m-p/2083328#M58101</link>
    <description>&lt;P&gt;I found a way which is very tricky. Finally I got about 37.5Mbytes/s(300Mbps).&lt;/P&gt;&lt;P&gt;I have to focus on the EndPoint buffer size. it should be 4Kbytes(This is a maximum I think in 8Kbytes USB SRAM).&lt;/P&gt;&lt;P&gt;And I have to work around the complicated interrupt handler codes.&lt;/P&gt;&lt;P&gt;This issue can be closed.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Apr 2025 13:46:50 GMT</pubDate>
    <dc:creator>Lex2</dc:creator>
    <dc:date>2025-04-18T13:46:50Z</dc:date>
    <item>
      <title>Max throughput of LPC546xx MCU HS High Speed USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-throughput-of-LPC546xx-MCU-HS-High-Speed-USB/m-p/2082230#M58085</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;I am evaluating the dev LPCXpresso546xx board.&lt;BR /&gt;I am very interesting in high speed USB throughput of this dev board.&lt;BR /&gt;I am using dev_cdc_vcom_bm example code to evaluate the MCU.&lt;BR /&gt;I modified the example source code not to reply echo message in order to maximize USB OUT throughput(only for traffic from a host).&lt;BR /&gt;I measured the throughput by sending a binary file to /dev/ttyACMx.&lt;BR /&gt;Currently, I get the throughput is about 12.34MB/s(98.72Mbps). I need at least 24MB/s.&amp;nbsp;&lt;BR /&gt;I wonder if a max throughput of this MCU is 12~15MB/s or not.&amp;nbsp;&lt;BR /&gt;I wonder if there are some modification points to increase the throughput or not.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Lex&lt;/P&gt;</description>
      <pubDate>Thu, 17 Apr 2025 05:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-throughput-of-LPC546xx-MCU-HS-High-Speed-USB/m-p/2082230#M58085</guid>
      <dc:creator>Lex2</dc:creator>
      <dc:date>2025-04-17T05:45:32Z</dc:date>
    </item>
    <item>
      <title>Re: Max throughput of LPC546xx MCU HS High Speed USB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Max-throughput-of-LPC546xx-MCU-HS-High-Speed-USB/m-p/2083328#M58101</link>
      <description>&lt;P&gt;I found a way which is very tricky. Finally I got about 37.5Mbytes/s(300Mbps).&lt;/P&gt;&lt;P&gt;I have to focus on the EndPoint buffer size. it should be 4Kbytes(This is a maximum I think in 8Kbytes USB SRAM).&lt;/P&gt;&lt;P&gt;And I have to work around the complicated interrupt handler codes.&lt;/P&gt;&lt;P&gt;This issue can be closed.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Apr 2025 13:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Max-throughput-of-LPC546xx-MCU-HS-High-Speed-USB/m-p/2083328#M58101</guid>
      <dc:creator>Lex2</dc:creator>
      <dc:date>2025-04-18T13:46:50Z</dc:date>
    </item>
  </channel>
</rss>