<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S28 USB HS Receiver sensitivity Test in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-HS-Receiver-sensitivity-Test/m-p/2078956#M58046</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244170"&gt;@hskating&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-qzbcQC paragraph-element br-paragraph-space"&gt;Please check the hardware as follows:&lt;/DIV&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-qzbcQC paragraph-element br-paragraph-space"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;Check the D+/D- differential lines. Ensure they are kept away from high - frequency sources such as clock lines and power switches.&lt;/P&gt;
&lt;P&gt;Please check the capacitor on the USB_VDD pin. Place it close to the chip. You can refer to the schematic of the lpcxpresso55s28 - evk board.&lt;/P&gt;
&lt;P&gt;Allocate a separate ground layer for the USB PHY.&lt;/P&gt;
&lt;P&gt;You can also use a USB analyzer to monitor the communication process signal.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Fri, 11 Apr 2025 09:23:21 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2025-04-11T09:23:21Z</dc:date>
    <item>
      <title>LPC55S28 USB HS Receiver sensitivity Test</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-HS-Receiver-sensitivity-Test/m-p/2074949#M58017</link>
      <description>&lt;P&gt;NXP team&lt;BR /&gt;When I used the LPC55S28 chip to make a product using high-speed usb, after the software function was basically completed, I began to conduct USB authentication Test, and encountered a problem about the Receiver sensitivity Test Reference. It looks something like this:&lt;BR /&gt;usb2.0 electrical test failure: High-speed devices must implement a transmission envelope detector that does not display suppression (that is, reliably receive packets) when the receiver differential amplitude exceeds 150mV.&lt;BR /&gt;Pass limit: &amp;lt;= 200.000 mVDevice&lt;BR /&gt;Please see the attachment for details.&lt;/P&gt;&lt;P&gt;How do I fix this?&lt;BR /&gt;I sincerely hope that the NXP team can give me advice and support in this regard.&lt;BR /&gt;Thank you from the bottom of my heart.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 08:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-HS-Receiver-sensitivity-Test/m-p/2074949#M58017</guid>
      <dc:creator>hskating</dc:creator>
      <dc:date>2025-04-07T08:13:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28 USB HS Receiver sensitivity Test</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-HS-Receiver-sensitivity-Test/m-p/2078956#M58046</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244170"&gt;@hskating&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-qzbcQC paragraph-element br-paragraph-space"&gt;Please check the hardware as follows:&lt;/DIV&gt;
&lt;DIV class="auto-hide-last-sibling-br paragraph-qzbcQC paragraph-element br-paragraph-space"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;Check the D+/D- differential lines. Ensure they are kept away from high - frequency sources such as clock lines and power switches.&lt;/P&gt;
&lt;P&gt;Please check the capacitor on the USB_VDD pin. Place it close to the chip. You can refer to the schematic of the lpcxpresso55s28 - evk board.&lt;/P&gt;
&lt;P&gt;Allocate a separate ground layer for the USB PHY.&lt;/P&gt;
&lt;P&gt;You can also use a USB analyzer to monitor the communication process signal.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 11 Apr 2025 09:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-USB-HS-Receiver-sensitivity-Test/m-p/2078956#M58046</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-04-11T09:23:21Z</dc:date>
    </item>
  </channel>
</rss>