<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC178x: UART 38400bps with 12MHz IRC</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC178x-UART-38400bps-with-12MHz-IRC/m-p/2075221#M58019</link>
    <description>&lt;P&gt;I need to create a RS485/UART communication link between LPC178X and SAMD20 MCU. The communication should be 38400bps.&lt;/P&gt;&lt;P&gt;The clock on SAMD20 is based on an external 32.768kHz crystal (XOSC32K) and DFLL in closed loop mode.&lt;/P&gt;&lt;P&gt;I'm wondering if it is possible to clock LPC178X with internal IRC 12MHz oscillator. The datasheet reports a precision of 1% (11.88-12.12MHz) over all the voltages and temperatures. It seems sufficient for UART communication that usually needs a maximum of 2% error.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Apr 2025 14:18:33 GMT</pubDate>
    <dc:creator>giusloq</dc:creator>
    <dc:date>2025-04-07T14:18:33Z</dc:date>
    <item>
      <title>LPC178x: UART 38400bps with 12MHz IRC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC178x-UART-38400bps-with-12MHz-IRC/m-p/2075221#M58019</link>
      <description>&lt;P&gt;I need to create a RS485/UART communication link between LPC178X and SAMD20 MCU. The communication should be 38400bps.&lt;/P&gt;&lt;P&gt;The clock on SAMD20 is based on an external 32.768kHz crystal (XOSC32K) and DFLL in closed loop mode.&lt;/P&gt;&lt;P&gt;I'm wondering if it is possible to clock LPC178X with internal IRC 12MHz oscillator. The datasheet reports a precision of 1% (11.88-12.12MHz) over all the voltages and temperatures. It seems sufficient for UART communication that usually needs a maximum of 2% error.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 14:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC178x-UART-38400bps-with-12MHz-IRC/m-p/2075221#M58019</guid>
      <dc:creator>giusloq</dc:creator>
      <dc:date>2025-04-07T14:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC178x: UART 38400bps with 12MHz IRC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC178x-UART-38400bps-with-12MHz-IRC/m-p/2076478#M58026</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160419"&gt;@giusloq&lt;/a&gt;,&lt;BR /&gt;I understand that you would use the IRC as core source clock, it is possible, as mentioned in the chapter 1.2 called "Features", as shown in the next image:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Habib_MS_0-1744146716879.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/332040iE4DC8D20490A97EE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Habib_MS_0-1744146716879.png" alt="Habib_MS_0-1744146716879.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Habib_MS_0-1744146716879.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Also, if you experience any issue do not hesitate to let me know&lt;BR /&gt;BR&lt;BR /&gt;Habib.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 21:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC178x-UART-38400bps-with-12MHz-IRC/m-p/2076478#M58026</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-04-08T21:12:11Z</dc:date>
    </item>
  </channel>
</rss>