<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with USB Mass Storage Device when executing from SPIFI on LPC1850 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-USB-Mass-Storage-Device-when-executing-from-SPIFI/m-p/523158#M5794</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by j.daheron on Fri Jul 27 01:11:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm developing a Mass Storage Device application using nxpUSBlib v0.95 running on LPC1850 (Keil MCB1800 Dev. Board).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I work on example code provided with the library, but I've changed the virtual disk to be in RAM area (some kB only).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The application works fine when running from RAM (like in the example), but the device is not recognized when the application runs from SPIFI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help me to understand why ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Julien&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:42:46 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:42:46Z</dc:date>
    <item>
      <title>Problem with USB Mass Storage Device when executing from SPIFI on LPC1850</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-USB-Mass-Storage-Device-when-executing-from-SPIFI/m-p/523158#M5794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by j.daheron on Fri Jul 27 01:11:00 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm developing a Mass Storage Device application using nxpUSBlib v0.95 running on LPC1850 (Keil MCB1800 Dev. Board).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I work on example code provided with the library, but I've changed the virtual disk to be in RAM area (some kB only).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The application works fine when running from RAM (like in the example), but the device is not recognized when the application runs from SPIFI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help me to understand why ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;--&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Julien&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:42:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-USB-Mass-Storage-Device-when-executing-from-SPIFI/m-p/523158#M5794</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:42:46Z</dc:date>
    </item>
  </channel>
</rss>