<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC552X SED pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552X-SED-pin/m-p/2063532#M57922</link>
    <description>&lt;P&gt;Greetings!&lt;/P&gt;&lt;P&gt;On P145 of UM11126, there is this paragraph&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;This mechanism is mainly used to recover a part programmed with a corrupted&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;image. For instance, on boards/products where the ISP pin mechanism in not&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;affordable and SED pins are accessible or when ISP mode is disabled through the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;“Default ISP mode” field in the CMPA_BOOT_CFG configuration word&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;What is SED pin? The doc or datasheet does not explain it anywhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Tue, 18 Mar 2025 07:31:02 GMT</pubDate>
    <dc:creator>steve5528</dc:creator>
    <dc:date>2025-03-18T07:31:02Z</dc:date>
    <item>
      <title>LPC552X SED pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552X-SED-pin/m-p/2063532#M57922</link>
      <description>&lt;P&gt;Greetings!&lt;/P&gt;&lt;P&gt;On P145 of UM11126, there is this paragraph&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;EM&gt;This mechanism is mainly used to recover a part programmed with a corrupted&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;image. For instance, on boards/products where the ISP pin mechanism in not&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;affordable and SED pins are accessible or when ISP mode is disabled through the&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;“Default ISP mode” field in the CMPA_BOOT_CFG configuration word&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;What is SED pin? The doc or datasheet does not explain it anywhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 07:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552X-SED-pin/m-p/2063532#M57922</guid>
      <dc:creator>steve5528</dc:creator>
      <dc:date>2025-03-18T07:31:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC552X SED pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552X-SED-pin/m-p/2065465#M57941</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246045"&gt;@steve5528&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your question.&lt;/P&gt;
&lt;P&gt;Sorry, this is a typo. It should be SWD.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Mar 2025 09:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC552X-SED-pin/m-p/2065465#M57941</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-03-20T09:52:06Z</dc:date>
    </item>
  </channel>
</rss>