<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1768 wake up from DeepSleep when bootloader is present</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2063509#M57921</link>
    <description>&lt;P&gt;I have a cusotm board with LPC1768 and I need to use deep sleep mode. Everything works OK as default but when I install a bootloader and the main program where I need to use deep sleep has an offset, when I wake up the MCU it clear ctach teh IRQ and wake up as current increased it remains stucked somewhere... possible goes on a wrong address. I do nto know how to debug as debuger does not work in deep sleep.&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 18 Mar 2025 06:44:54 GMT</pubDate>
    <dc:creator>laurianussss</dc:creator>
    <dc:date>2025-03-18T06:44:54Z</dc:date>
    <item>
      <title>LPC1768 wake up from DeepSleep when bootloader is present</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2063509#M57921</link>
      <description>&lt;P&gt;I have a cusotm board with LPC1768 and I need to use deep sleep mode. Everything works OK as default but when I install a bootloader and the main program where I need to use deep sleep has an offset, when I wake up the MCU it clear ctach teh IRQ and wake up as current increased it remains stucked somewhere... possible goes on a wrong address. I do nto know how to debug as debuger does not work in deep sleep.&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 06:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2063509#M57921</guid>
      <dc:creator>laurianussss</dc:creator>
      <dc:date>2025-03-18T06:44:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 wake up from DeepSleep when bootloader is present</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2064126#M57929</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247325"&gt;@laurianussss&lt;/a&gt;,&lt;BR /&gt;Could you execute the Bootloader application and the low power mode independently?&amp;nbsp;this with the propose of corroborate that both work as expected.&lt;/P&gt;
&lt;P&gt;Also, I highly recommend see the 4.8.2 called " Deep Sleep mode" in order to obtain more information about low power mode.&lt;/P&gt;
&lt;P&gt;BR&lt;BR /&gt;Habib&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 22:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2064126#M57929</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2025-03-18T22:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 wake up from DeepSleep when bootloader is present</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2064191#M57932</link>
      <description>&lt;P&gt;Yes... aplicatiopn was aorking independently. Anyway I found the problem and solution. Only need it to add Offset address when reainitialize the clock&amp;nbsp;&lt;/P&gt;&lt;P&gt;SCB-&amp;gt;VTOR = ADRE_OFFSET &amp;amp; 0x3FFFFF80;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 01:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-wake-up-from-DeepSleep-when-bootloader-is-present/m-p/2064191#M57932</guid>
      <dc:creator>laurianussss</dc:creator>
      <dc:date>2025-03-19T01:27:44Z</dc:date>
    </item>
  </channel>
</rss>