<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC 1768 CRP3 Enabled Device Recover</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1768-CRP3-Enabled-Device-Recover/m-p/2060510#M57886</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using LPC1768 with CRP3 is enabled in the code for security purpose.&lt;/P&gt;&lt;P&gt;But due to some FOTA issue our Application is got corrupted and not running.&lt;/P&gt;&lt;P&gt;We want to recover this Device's either JTAG or ISP Mode.&lt;/P&gt;&lt;P&gt;Since CRP3 is enabled , LPC1768 not allowing JTAG and ISP Mode.&lt;/P&gt;&lt;P&gt;Please any suggestion to Recover those Device's.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Mar 2025 14:22:38 GMT</pubDate>
    <dc:creator>vijayg</dc:creator>
    <dc:date>2025-03-12T14:22:38Z</dc:date>
    <item>
      <title>LPC 1768 CRP3 Enabled Device Recover</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1768-CRP3-Enabled-Device-Recover/m-p/2060510#M57886</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using LPC1768 with CRP3 is enabled in the code for security purpose.&lt;/P&gt;&lt;P&gt;But due to some FOTA issue our Application is got corrupted and not running.&lt;/P&gt;&lt;P&gt;We want to recover this Device's either JTAG or ISP Mode.&lt;/P&gt;&lt;P&gt;Since CRP3 is enabled , LPC1768 not allowing JTAG and ISP Mode.&lt;/P&gt;&lt;P&gt;Please any suggestion to Recover those Device's.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 14:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1768-CRP3-Enabled-Device-Recover/m-p/2060510#M57886</guid>
      <dc:creator>vijayg</dc:creator>
      <dc:date>2025-03-12T14:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 1768 CRP3 Enabled Device Recover</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1768-CRP3-Enabled-Device-Recover/m-p/2060836#M57889</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247482"&gt;@vijayg&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I don’t believe the device can be recovered because, at the CRP3 level, both ISP&amp;nbsp; pin and SWD&amp;nbsp; are disabled.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Be aware that there is no built-in recovery for designs once CRP Level 3 is enabled. The most simplistic way of implementing a custom recovery mechanism involves the “Re-Invoke ISP” IAP call.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="888888888888.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/327828i57BD5C578CB584D3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="888888888888.jpg" alt="888888888888.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;888888888888.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Thu, 13 Mar 2025 02:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1768-CRP3-Enabled-Device-Recover/m-p/2060836#M57889</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-03-13T02:18:22Z</dc:date>
    </item>
  </channel>
</rss>