<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Assistance Required for CAN 1 Configuration on LPC54606J512 MCU in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Assistance-Required-for-CAN-1-Configuration-on-LPC54606J512-MCU/m-p/2054336#M57797</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247431"&gt;@amit_sutrave77&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;First, you should check the Hardware Connections and&amp;nbsp; Verify Clock and Baud Rate Configuration.&lt;/P&gt;
&lt;P&gt;And then&amp;nbsp;I think you can try a simple internal loopback test to confirm that CAN transmission and reception work without a transceiver.&lt;BR /&gt;&lt;BR /&gt;Use an oscilloscope or logic analyzer to check if CAN_TD is sending data.&lt;BR /&gt;&lt;BR /&gt;Capture error codes from the CAN error status registers.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
    <pubDate>Mon, 03 Mar 2025 03:41:18 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2025-03-03T03:41:18Z</dc:date>
    <item>
      <title>Assistance Required for CAN 1 Configuration on LPC54606J512 MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Assistance-Required-for-CAN-1-Configuration-on-LPC54606J512-MCU/m-p/2053025#M57777</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;I am working with the LPC54606J512 MCU and am trying to use CAN 1. I have configured the CAN_TD and CAN_RD pins, but I am encountering the error "kStatus_MCAN_ErrorStatus" when transmitting data. Below are the configurations I have changed for CAN 1:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;#define USE_IMPROVED_TIMING_CONFIG (1U)
#define EXAMPLE_MCAN_IRQHandler CAN1_IRQ0_IRQHandler
#define EXAMPLE_MCAN_IRQn CAN1_IRQ0_IRQn
#define EXAMPLE_MCAN CAN1
#define MCAN_CLK_FREQ CLOCK_GetMCanClkFreq(1U)&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;The clock frequency is set to 12 MHz, with the following configuration:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;config-&amp;gt;baudRateA = 500000U;
config-&amp;gt;baudRateD = 2000000U;
config-&amp;gt;enableCanfdNormal = false;
config-&amp;gt;enableCanfdSwitch = false;
config-&amp;gt;enableLoopBackInt = false;
config-&amp;gt;enableLoopBackExt = false;
config-&amp;gt;enableBusMon = false;
/* Default protocol timing configuration, time quantum is 16. */
config-&amp;gt;timingConfig.seg1 = 0xAU;
config-&amp;gt;timingConfig.seg2 = 0x3U;
config-&amp;gt;timingConfig.rJumpwidth = 0x3U;&lt;/LI-CODE&gt;&lt;P&gt;Could you kindly guide me in resolving this issue.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;BR /&gt;Amit Sutrave&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220926"&gt;@a_s&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 14:33:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Assistance-Required-for-CAN-1-Configuration-on-LPC54606J512-MCU/m-p/2053025#M57777</guid>
      <dc:creator>amit_sutrave77</dc:creator>
      <dc:date>2025-02-27T14:33:04Z</dc:date>
    </item>
    <item>
      <title>Re: Assistance Required for CAN 1 Configuration on LPC54606J512 MCU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Assistance-Required-for-CAN-1-Configuration-on-LPC54606J512-MCU/m-p/2054336#M57797</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247431"&gt;@amit_sutrave77&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;First, you should check the Hardware Connections and&amp;nbsp; Verify Clock and Baud Rate Configuration.&lt;/P&gt;
&lt;P&gt;And then&amp;nbsp;I think you can try a simple internal loopback test to confirm that CAN transmission and reception work without a transceiver.&lt;BR /&gt;&lt;BR /&gt;Use an oscilloscope or logic analyzer to check if CAN_TD is sending data.&lt;BR /&gt;&lt;BR /&gt;Capture error codes from the CAN error status registers.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 03:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Assistance-Required-for-CAN-1-Configuration-on-LPC54606J512-MCU/m-p/2054336#M57797</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-03-03T03:41:18Z</dc:date>
    </item>
  </channel>
</rss>