<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC5536 Flexcomm Voltage Rails</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-Flexcomm-Voltage-Rails/m-p/2050262#M57745</link>
    <description>&lt;P&gt;Unfortunately, this is chip design. I apologize for the inconvenience this may cause you.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 24 Feb 2025 22:11:01 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2025-02-24T22:11:01Z</dc:date>
    <item>
      <title>LPC5536 Flexcomm Voltage Rails</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-Flexcomm-Voltage-Rails/m-p/2047295#M57717</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;on the LPC5536 64 Pin Package. I want to use 3.3V on VDDIO_1 and 1.8V on VDDIO_2 but it seems like there is no Flexcomm Peripheral that has all 4 SPI Signals within a single Voltage Domain.&lt;/P&gt;&lt;P&gt;They are always split up between VDDIO_1 and VDDIO_2 ... am i missing something or is this intentional ??&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 12:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-Flexcomm-Voltage-Rails/m-p/2047295#M57717</guid>
      <dc:creator>mf89</dc:creator>
      <dc:date>2025-02-19T12:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5536 Flexcomm Voltage Rails</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-Flexcomm-Voltage-Rails/m-p/2050262#M57745</link>
      <description>&lt;P&gt;Unfortunately, this is chip design. I apologize for the inconvenience this may cause you.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 22:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5536-Flexcomm-Voltage-Rails/m-p/2050262#M57745</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-02-24T22:11:01Z</dc:date>
    </item>
  </channel>
</rss>