<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S6X USB0 in host mode in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049888#M57743</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&amp;nbsp; I'll look into the resources you have provided.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regd. you comment "&lt;SPAN&gt;The USB0_VBUS should be connected to 5V" --&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;on p44,&amp;nbsp;Rev. 2.3 of&amp;nbsp;LPC55S2X_LPC552X datasheet it states the following:&lt;/P&gt;&lt;P&gt;[6]&lt;BR /&gt;The corresponding VBUS must be connected to supply voltage when using the USB peripheral. USB0_VBUS is not 5 V tolerant pin and is tolerant up to&lt;BR /&gt;3.6 V only when the VDD is at operating level (minimum: 1.8 V). USB1_VBUS is 5 V tolerant pin regardless if the VDD supply is present or not.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;it doesn't talk about the host mode, but still it is confusing - that was the reason for me to think it needs to be connected to 3v3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Feb 2025 11:58:14 GMT</pubDate>
    <dc:creator>manuela_mendez</dc:creator>
    <dc:date>2025-02-24T11:58:14Z</dc:date>
    <item>
      <title>LPC55S6X USB0 in host mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049473#M57736</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello NXP Experts,&lt;/P&gt;&lt;P&gt;I've few clarification questions on using USB0 as host on LPC55S6x:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;UM11126, rev2.7, p832 table 780 says: &lt;U&gt;"Enable USB0_VBUS pin for correct host operation. For example, it is required detect a change in the connection status."&lt;/U&gt;&amp;nbsp;&lt;OL&gt;&lt;LI&gt;what is the correct way to achieve this? can VBUS0_VBUS be tied permanently to 3.3v?&lt;/LI&gt;&lt;LI&gt;what is the pullup recommendation to minimize the current draw? is there anything else required at the schematic level?&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;Could you explain USB0_VBUS role in host mode? LPC55x documentation has no coverage on this. Is there an older MCU doc that talks about this?&lt;/LI&gt;&lt;LI&gt;Does LPC55S6X-EVK support using USB0 as host? I see this being exposed as PIO22 on the headers, but not sure what else is needs to be done to get the host functional&lt;/LI&gt;&lt;LI&gt;Is there a SDK example that uses USB0 has host?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Sun, 23 Feb 2025 14:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049473#M57736</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-02-23T14:50:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6X USB0 in host mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049828#M57742</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245216"&gt;@manuela_mendez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;UL class="auto-hide-last-sibling-br"&gt;
&lt;LI&gt;The USB0_VBUS should be connected to 5V.&lt;/LI&gt;
&lt;LI&gt;When USB0 functions as a host, the USB0_VBUS is used to supply power to the USB device and also to detect whether the device is connected or disconnected.&lt;/LI&gt;
&lt;LI&gt;The LPC55s6x-EVK supports USB0 as a host. Please refer to the LPCXpresso55s69 User Manual for configuring the hardware. Hardware please refer to schematic of lpcxpresso55s69-evk.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LPC55S69-SCH" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=LPC55S69-SCH&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.jpg" style="width: 705px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325336i11DD4678969C01B3/image-size/large?v=v2&amp;amp;px=999" role="button" title="3.jpg" alt="3.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="4.jpg" style="width: 726px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325337i7AD6A46DABDEE29F/image-size/large?v=v2&amp;amp;px=999" role="button" title="4.jpg" alt="4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;UL class="auto-hide-last-sibling-br"&gt;
&lt;LI&gt;The USB host example uses USB0 by default. Please refer to the relevant documentation for further details.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 10:17:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049828#M57742</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-02-24T10:17:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6X USB0 in host mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049888#M57743</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&amp;nbsp; I'll look into the resources you have provided.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regd. you comment "&lt;SPAN&gt;The USB0_VBUS should be connected to 5V" --&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;on p44,&amp;nbsp;Rev. 2.3 of&amp;nbsp;LPC55S2X_LPC552X datasheet it states the following:&lt;/P&gt;&lt;P&gt;[6]&lt;BR /&gt;The corresponding VBUS must be connected to supply voltage when using the USB peripheral. USB0_VBUS is not 5 V tolerant pin and is tolerant up to&lt;BR /&gt;3.6 V only when the VDD is at operating level (minimum: 1.8 V). USB1_VBUS is 5 V tolerant pin regardless if the VDD supply is present or not.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;it doesn't talk about the host mode, but still it is confusing - that was the reason for me to think it needs to be connected to 3v3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 11:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2049888#M57743</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-02-24T11:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6X USB0 in host mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2051410#M57763</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245216"&gt;@manuela_mendez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you are right. So design USB0_VBUS as below:&lt;/P&gt;
&lt;DIV id="tinyMceEditorAlice_Yang_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="33333.jpg" style="width: 779px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325702i768FA100FDCBC720/image-size/large?v=v2&amp;amp;px=999" role="button" title="33333.jpg" alt="33333.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 06:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2051410#M57763</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-02-26T06:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6X USB0 in host mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2052161#M57768</link>
      <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;: thank you for the confirmation!</description>
      <pubDate>Wed, 26 Feb 2025 20:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6X-USB0-in-host-mode/m-p/2052161#M57768</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-02-26T20:23:45Z</dc:date>
    </item>
  </channel>
</rss>