<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックNXP I2C Application Note stating the maximum byte transfer</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2048620#M57728</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;Is there an existing I2C Device who can handle more than 255bytes in one Single Transaction?&lt;/P&gt;&lt;P&gt;Please share an application note or literature if this is not possible.&lt;/P&gt;&lt;P&gt;Thanks and Good Day,&lt;/P&gt;&lt;P&gt;Leo&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 21 Feb 2025 00:17:17 GMT</pubDate>
    <dc:creator>lpestanas</dc:creator>
    <dc:date>2025-02-21T00:17:17Z</dc:date>
    <item>
      <title>NXP I2C Application Note stating the maximum byte transfer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2048620#M57728</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;Is there an existing I2C Device who can handle more than 255bytes in one Single Transaction?&lt;/P&gt;&lt;P&gt;Please share an application note or literature if this is not possible.&lt;/P&gt;&lt;P&gt;Thanks and Good Day,&lt;/P&gt;&lt;P&gt;Leo&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 00:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2048620#M57728</guid>
      <dc:creator>lpestanas</dc:creator>
      <dc:date>2025-02-21T00:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: NXP I2C Application Note stating the maximum byte transfer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2049778#M57739</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217592"&gt;@lpestanas&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The standard I2C devices are generally limited by the 255-byte payload size per transaction due to the I2C protocol's use of an 8-bit register for data length.&lt;/P&gt;
&lt;DIV id="tinyMceEditorHarry_Zhang_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2025-02-24_17-27-28.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325324iF53AECDD6C41AD2C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snipaste_2025-02-24_17-27-28.png" alt="Snipaste_2025-02-24_17-27-28.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Snipaste_2025-02-24_17-27-00.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/325323i0901B21A81E1007B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Snipaste_2025-02-24_17-27-00.png" alt="Snipaste_2025-02-24_17-27-00.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;To handle more than 255 bytes in one transaction, you can Use Multiple Transactions.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 09:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2049778#M57739</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-02-24T09:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: NXP I2C Application Note stating the maximum byte transfer</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2049795#M57741</link>
      <description>Hi Harry,&lt;BR /&gt;&lt;BR /&gt;Thanks, it means that I need to use multiple transactions to divide an input write of 4kB for example.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Leo</description>
      <pubDate>Mon, 24 Feb 2025 09:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NXP-I2C-Application-Note-stating-the-maximum-byte-transfer/m-p/2049795#M57741</guid>
      <dc:creator>lpestanas</dc:creator>
      <dc:date>2025-02-24T09:50:23Z</dc:date>
    </item>
  </channel>
</rss>