<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC553x I3C PUR Signal availability in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-I3C-PUR-Signal-availability/m-p/2046551#M57707</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the LPC553x MCU Features a Hardware I3C Peripheral. Is the "PUR" Pull Up resistor control Pin only available in the 100 Pin Package ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If yes is there an alternative solution for the 64 and 48 Pin Package to handle external Pull Ups on SDA line ?&lt;/P&gt;</description>
    <pubDate>Tue, 18 Feb 2025 17:45:48 GMT</pubDate>
    <dc:creator>mf89</dc:creator>
    <dc:date>2025-02-18T17:45:48Z</dc:date>
    <item>
      <title>LPC553x I3C PUR Signal availability</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-I3C-PUR-Signal-availability/m-p/2046551#M57707</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the LPC553x MCU Features a Hardware I3C Peripheral. Is the "PUR" Pull Up resistor control Pin only available in the 100 Pin Package ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If yes is there an alternative solution for the 64 and 48 Pin Package to handle external Pull Ups on SDA line ?&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 17:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-I3C-PUR-Signal-availability/m-p/2046551#M57707</guid>
      <dc:creator>mf89</dc:creator>
      <dc:date>2025-02-18T17:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC553x I3C PUR Signal availability</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-I3C-PUR-Signal-availability/m-p/2046604#M57710</link>
      <description>&lt;P&gt;Yes, only 100-pin package has PUR pin on external SDA pull-up, for smaller package, you have to configure a pin as GPIO and toggle it to control the external SDA pull-up. It's meant for a strong pull-up, not sure if it's always needed depending on your application.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 19:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC553x-I3C-PUR-Signal-availability/m-p/2046604#M57710</guid>
      <dc:creator>Dezheng_Tang</dc:creator>
      <dc:date>2025-02-18T19:29:14Z</dc:date>
    </item>
  </channel>
</rss>