<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 zephyr usbhs Sleep and wake up functions are not supported</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2044193#M57686</link>
    <description>&lt;P&gt;I tested this example while debugging LPC55s28: samples/subsys/usb/hid-mouse CONFIG_USB_DEVICE_REMOTE_WAKEUP=y was set in samples/subsys/usb/hid-mouse/prj.conf, but after compiling the project: int usb_dc_wakeup_request(void) is not supported in drivers/usb/device/usb_dc_mcux.c; Please tell me how to solve this. I also used MCUXpressoIDE to generate a copy of lpcxpresso55s28_dev_suspend_resume_hid_mouse_bm\source\mouse.c, However, it is not possible to add examples to drivers/usb/device/usb_dc_mcux.c in zephyr. I think this also needs to support low power control. Is there a successful example in zephyr? Thank you very much.&lt;/P&gt;</description>
    <pubDate>Fri, 14 Feb 2025 03:33:35 GMT</pubDate>
    <dc:creator>hskating</dc:creator>
    <dc:date>2025-02-14T03:33:35Z</dc:date>
    <item>
      <title>zephyr usbhs Sleep and wake up functions are not supported</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2044193#M57686</link>
      <description>&lt;P&gt;I tested this example while debugging LPC55s28: samples/subsys/usb/hid-mouse CONFIG_USB_DEVICE_REMOTE_WAKEUP=y was set in samples/subsys/usb/hid-mouse/prj.conf, but after compiling the project: int usb_dc_wakeup_request(void) is not supported in drivers/usb/device/usb_dc_mcux.c; Please tell me how to solve this. I also used MCUXpressoIDE to generate a copy of lpcxpresso55s28_dev_suspend_resume_hid_mouse_bm\source\mouse.c, However, it is not possible to add examples to drivers/usb/device/usb_dc_mcux.c in zephyr. I think this also needs to support low power control. Is there a successful example in zephyr? Thank you very much.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Feb 2025 03:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2044193#M57686</guid>
      <dc:creator>hskating</dc:creator>
      <dc:date>2025-02-14T03:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: zephyr usbhs Sleep and wake up functions are not supported</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2045925#M57700</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244170"&gt;@hskating&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry,&amp;nbsp; we currently do not support USB low power control on&amp;nbsp;LPC55s28 Zephyr.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 04:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2045925#M57700</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-02-18T04:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: zephyr usbhs Sleep and wake up functions are not supported</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2046170#M57702</link>
      <description>&lt;P&gt;Will nxp mcu with usb support zephyr with low power consumption in the future?&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 08:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/zephyr-usbhs-Sleep-and-wake-up-functions-are-not-supported/m-p/2046170#M57702</guid>
      <dc:creator>hskating</dc:creator>
      <dc:date>2025-02-18T08:58:00Z</dc:date>
    </item>
  </channel>
</rss>