<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPCXpresso54628 Development Board SDRAM addressing in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Development-Board-SDRAM-addressing/m-p/2041201#M57661</link>
    <description>&lt;P&gt;I am using the documentation for the LPCXpress54628 development board as a guide to replicate the interface with the SDRAM IC IS42S16800F-6BLI in my own design.&amp;nbsp; I noticed on the diagram that there is a&amp;nbsp;P1_24-EMC_A12 identified connected to pin G1.&amp;nbsp; However, the datasheet for that device shows pin G1 as NC.&amp;nbsp; I will assume it really isn't a functioning connection.&amp;nbsp; The 12 address lines A0-A11 do provide the 4K of addressing for the memory.&amp;nbsp; Was there a part change?&amp;nbsp; The other part number (W9812G6JB) also shows NC on G1.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;</description>
    <pubDate>Mon, 10 Feb 2025 22:05:16 GMT</pubDate>
    <dc:creator>samv</dc:creator>
    <dc:date>2025-02-10T22:05:16Z</dc:date>
    <item>
      <title>LPCXpresso54628 Development Board SDRAM addressing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Development-Board-SDRAM-addressing/m-p/2041201#M57661</link>
      <description>&lt;P&gt;I am using the documentation for the LPCXpress54628 development board as a guide to replicate the interface with the SDRAM IC IS42S16800F-6BLI in my own design.&amp;nbsp; I noticed on the diagram that there is a&amp;nbsp;P1_24-EMC_A12 identified connected to pin G1.&amp;nbsp; However, the datasheet for that device shows pin G1 as NC.&amp;nbsp; I will assume it really isn't a functioning connection.&amp;nbsp; The 12 address lines A0-A11 do provide the 4K of addressing for the memory.&amp;nbsp; Was there a part change?&amp;nbsp; The other part number (W9812G6JB) also shows NC on G1.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 22:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Development-Board-SDRAM-addressing/m-p/2041201#M57661</guid>
      <dc:creator>samv</dc:creator>
      <dc:date>2025-02-10T22:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54628 Development Board SDRAM addressing</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Development-Board-SDRAM-addressing/m-p/2041703#M57666</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/89562"&gt;@samv&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, The W9812G6JB&lt;/SPAN&gt; and &lt;SPAN&gt;IS42S16800F-6BLI&lt;/SPAN&gt; both have only 12 bit address lines.&lt;/P&gt;
&lt;P&gt;They are&amp;nbsp;128Mb SDRAM.&lt;/P&gt;
&lt;P&gt;You can also check the LPC54628 RM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1739270013304.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323398i130D56BF8FB721F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1739270013304.png" alt="Harry_Zhang_0-1739270013304.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 10:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Development-Board-SDRAM-addressing/m-p/2041703#M57666</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-02-11T10:33:46Z</dc:date>
    </item>
  </channel>
</rss>