<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Flexcomm serial single pin TXD usage</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flexcomm-serial-single-pin-TXD-usage/m-p/2039807#M57648</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I don't have much experience in configuring Flexcomm and pin ports for LPC5504. I have the pin FC3_TXD_SCL_MISO_WS available but the rest of the FC3 serial port pins are being used as simple PIO/ Digital Input Output pins (Function=0).&lt;/P&gt;&lt;P&gt;I was wondering if it is possible to use only the Flexcomm 3 TXD pin for&amp;nbsp; communication (basically sending debug information) while keeping the rest of the pins for other functions like DIO.&lt;/P&gt;</description>
    <pubDate>Fri, 07 Feb 2025 08:43:44 GMT</pubDate>
    <dc:creator>pejo</dc:creator>
    <dc:date>2025-02-07T08:43:44Z</dc:date>
    <item>
      <title>Flexcomm serial single pin TXD usage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flexcomm-serial-single-pin-TXD-usage/m-p/2039807#M57648</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I don't have much experience in configuring Flexcomm and pin ports for LPC5504. I have the pin FC3_TXD_SCL_MISO_WS available but the rest of the FC3 serial port pins are being used as simple PIO/ Digital Input Output pins (Function=0).&lt;/P&gt;&lt;P&gt;I was wondering if it is possible to use only the Flexcomm 3 TXD pin for&amp;nbsp; communication (basically sending debug information) while keeping the rest of the pins for other functions like DIO.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 08:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flexcomm-serial-single-pin-TXD-usage/m-p/2039807#M57648</guid>
      <dc:creator>pejo</dc:creator>
      <dc:date>2025-02-07T08:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcomm serial single pin TXD usage</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flexcomm-serial-single-pin-TXD-usage/m-p/2040260#M57652</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232719"&gt;@pejo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, you can use only the FC3_TXD pin for communication while keeping the other Flexcomm 3 (FC3) pins as GPIO. The LPC5504 allows configuring individual pins for different functions within the Flexcomm peripheral, so you don’t need to enable the full UART interface.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Sat, 08 Feb 2025 02:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flexcomm-serial-single-pin-TXD-usage/m-p/2040260#M57652</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-02-08T02:07:01Z</dc:date>
    </item>
  </channel>
</rss>