<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCxpresso55s36 -EVK CAN hardware setup in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso55s36-EVK-CAN-hardware-setup/m-p/2038015#M57621</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244243"&gt;@madhubanti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If you follow the readme file of the mcan-interrupt transfer demo example and short JP23 and JP24, what you are doing is disabling CANH and CANL bus line. JP48 and JP49 on the default setting (Pins 1-2 shorted) set the target MCU MCAN controller receive and transmit to PIO1_3 and PIO1_2 respectively.&lt;/P&gt;
&lt;P&gt;See Table 6. LPCXpresso55S36 jumpers of LPCXpresso55S36 Development Board User Manual&lt;/P&gt;
&lt;P&gt;Checking the schematic you could see that PIO1_3 and PIO1_2 are on J92.&lt;/P&gt;
&lt;P&gt;Also, in order to complete the transmission two boards needs to be connected.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
    <pubDate>Tue, 04 Feb 2025 20:50:03 GMT</pubDate>
    <dc:creator>Pablo_Ramos</dc:creator>
    <dc:date>2025-02-04T20:50:03Z</dc:date>
    <item>
      <title>LPCxpresso55s36 -EVK CAN hardware setup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso55s36-EVK-CAN-hardware-setup/m-p/2035587#M57602</link>
      <description>&lt;P&gt;I am trying to run the mcan-interrupt transfer demo example. I connected the jumpers JP23 and JP24 to enable the CANH and CANL lines. But I am not able to successfully test the CAN working.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read J48 and J49 also needs to be aligned for operation. But I am confused as they are already have the pins shorted.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please guide me how to setup the CAN on the EVK board.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jan 2025 11:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso55s36-EVK-CAN-hardware-setup/m-p/2035587#M57602</guid>
      <dc:creator>madhubanti</dc:creator>
      <dc:date>2025-01-29T11:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso55s36 -EVK CAN hardware setup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso55s36-EVK-CAN-hardware-setup/m-p/2038015#M57621</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244243"&gt;@madhubanti&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If you follow the readme file of the mcan-interrupt transfer demo example and short JP23 and JP24, what you are doing is disabling CANH and CANL bus line. JP48 and JP49 on the default setting (Pins 1-2 shorted) set the target MCU MCAN controller receive and transmit to PIO1_3 and PIO1_2 respectively.&lt;/P&gt;
&lt;P&gt;See Table 6. LPCXpresso55S36 jumpers of LPCXpresso55S36 Development Board User Manual&lt;/P&gt;
&lt;P&gt;Checking the schematic you could see that PIO1_3 and PIO1_2 are on J92.&lt;/P&gt;
&lt;P&gt;Also, in order to complete the transmission two boards needs to be connected.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 20:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso55s36-EVK-CAN-hardware-setup/m-p/2038015#M57621</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-02-04T20:50:03Z</dc:date>
    </item>
  </channel>
</rss>