<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1765 secondary bootloader with USB MSD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-secondary-bootloader-with-USB-MSD/m-p/2037421#M57616</link>
    <description>&lt;P&gt;I suggest you comparing the linker of both projects, it is possible that the USB side is beign executed from flash while it needs to be excuted on RAM so it do not interfeeres with the erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Mon, 03 Feb 2025 22:46:10 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2025-02-03T22:46:10Z</dc:date>
    <item>
      <title>LPC1765 secondary bootloader with USB MSD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-secondary-bootloader-with-USB-MSD/m-p/2035278#M57596</link>
      <description>&lt;P&gt;We ported a secondary boot loader from LPCXpresso 8.2.2 to MCU expresso 24.9&lt;/P&gt;&lt;P&gt;The bootloader reads a bin file from a USB flash disk.&lt;/P&gt;&lt;P&gt;The USB stack is nxpUSBLib with FAT file system&lt;/P&gt;&lt;P&gt;The USB works fine and IAP&amp;nbsp; ommands works fine, but not together.&lt;/P&gt;&lt;P&gt;After erasing the flash the USB flashvdri e stops responding and the firmware hungs.while trying reading from USB. flash drive.&lt;/P&gt;&lt;P&gt;Everything worked fine with LPCXpresso 8.2.2&lt;/P&gt;&lt;P&gt;Any idea what we are missing?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jan 2025 20:15:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-secondary-bootloader-with-USB-MSD/m-p/2035278#M57596</guid>
      <dc:creator>Ronaa</dc:creator>
      <dc:date>2025-01-28T20:15:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1765 secondary bootloader with USB MSD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-secondary-bootloader-with-USB-MSD/m-p/2037421#M57616</link>
      <description>&lt;P&gt;I suggest you comparing the linker of both projects, it is possible that the USB side is beign executed from flash while it needs to be excuted on RAM so it do not interfeeres with the erase.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 03 Feb 2025 22:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1765-secondary-bootloader-with-USB-MSD/m-p/2037421#M57616</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2025-02-03T22:46:10Z</dc:date>
    </item>
  </channel>
</rss>