<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: S69 USB1 series termination</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2033742#M57577</link>
    <description>&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the response. Impedance matched USB cable is common to both USB0/USB1 cases so I suggest we leave that out of the discussion. Your response seems to indicate that USB1 controller on the chip is already impedance matched to 90ohm so it does not need series termination unlike USB0. Is this the correct interpretation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Fri, 24 Jan 2025 08:29:57 GMT</pubDate>
    <dc:creator>manuela_mendez</dc:creator>
    <dc:date>2025-01-24T08:29:57Z</dc:date>
    <item>
      <title>S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2028954#M57536</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In S69-EVK schematics, 33 ohm series resistors are included only for USB0 but not for USB1. In a previous response NXP recommended it for both; Could you clarify why USB1 does not have it in the schematic and when it is needed?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 10:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2028954#M57536</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-01-16T10:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2029297#M57542</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, let me get more details.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 21:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2029297#M57542</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2025-01-16T21:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2033485#M57575</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245216"&gt;@manuela_mendez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your patience, just kindly continuing the thread for my colleague Pavel, and the one from our&amp;nbsp;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-USB-questions/td-p/2022647" target="_self"&gt;previous response&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The LPC55s69 contains two USB interfaces:&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;-USB0 supporting Full-speed USB&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;-USB1 supportting High Speed USB.&lt;/P&gt;
&lt;P&gt;Therefore:&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;-The full-speed USB (USB0)needs the 33ohms .&amp;nbsp;&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;The&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;high-speed USB (USB1) connection is made through a shielded, twisted pair cable with a differential characteristic impedance of 90 Ω. In addition the USB1 is connected to the&amp;nbsp; internal USB 2.0 PHY, this will&amp;nbsp; do the impedance matching if necessary, therefore no external resistors are necessary.&amp;nbsp;You can find more information regarding the electrical specifications for the USB high speed by downloading the&amp;nbsp;&lt;A href="https://www.usb.org/document-library/usb-20-specification" target="_blank" rel="nofollow noopener noreferrer"&gt;USB 2.0 Specification&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;We hope this could help you!&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jan 2025 23:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2033485#M57575</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-01-23T23:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2033742#M57577</link>
      <description>&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the response. Impedance matched USB cable is common to both USB0/USB1 cases so I suggest we leave that out of the discussion. Your response seems to indicate that USB1 controller on the chip is already impedance matched to 90ohm so it does not need series termination unlike USB0. Is this the correct interpretation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jan 2025 08:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2033742#M57577</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-01-24T08:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2036371#M57606</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245216"&gt;@manuela_mendez&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;My apologies for the delayed response, I agree with your understanding.&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jan 2025 23:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2036371#M57606</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2025-01-30T23:59:44Z</dc:date>
    </item>
    <item>
      <title>Re: S69 USB1 series termination</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2036450#M57608</link>
      <description>Thanks Diego!</description>
      <pubDate>Fri, 31 Jan 2025 07:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/S69-USB1-series-termination/m-p/2036450#M57608</guid>
      <dc:creator>manuela_mendez</dc:creator>
      <dc:date>2025-01-31T07:27:34Z</dc:date>
    </item>
  </channel>
</rss>