<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using the Debug Mailbox with IAR tools in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-Debug-Mailbox-with-IAR-tools/m-p/2028999#M57539</link>
    <description>&lt;P&gt;I am using ISP through UART on LPC54605. I follow the procedure described in the User Manual, that is:&lt;/P&gt;&lt;P&gt;- send synchronization char&lt;/P&gt;&lt;P&gt;- send "Synchronized\r\n"&lt;/P&gt;&lt;P&gt;- send freq&lt;/P&gt;&lt;P&gt;After all this commands I am getting expected response. How ever, when I send Unlock command I am receiving ERR_ISP_PARAM_ERROR return code. Unlock commands which I am sending is structured as:&lt;/P&gt;&lt;P&gt;"U 23130\r\n"&lt;/P&gt;&lt;P&gt;Procedure, which I am using works on other LPC devices, such as LPC11Axx.&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 11:47:12 GMT</pubDate>
    <dc:creator>rony243</dc:creator>
    <dc:date>2025-01-16T11:47:12Z</dc:date>
    <item>
      <title>Using the Debug Mailbox with IAR tools</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-Debug-Mailbox-with-IAR-tools/m-p/2028999#M57539</link>
      <description>&lt;P&gt;I am using ISP through UART on LPC54605. I follow the procedure described in the User Manual, that is:&lt;/P&gt;&lt;P&gt;- send synchronization char&lt;/P&gt;&lt;P&gt;- send "Synchronized\r\n"&lt;/P&gt;&lt;P&gt;- send freq&lt;/P&gt;&lt;P&gt;After all this commands I am getting expected response. How ever, when I send Unlock command I am receiving ERR_ISP_PARAM_ERROR return code. Unlock commands which I am sending is structured as:&lt;/P&gt;&lt;P&gt;"U 23130\r\n"&lt;/P&gt;&lt;P&gt;Procedure, which I am using works on other LPC devices, such as LPC11Axx.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 11:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-Debug-Mailbox-with-IAR-tools/m-p/2028999#M57539</guid>
      <dc:creator>rony243</dc:creator>
      <dc:date>2025-01-16T11:47:12Z</dc:date>
    </item>
    <item>
      <title>Re: Using the Debug Mailbox with IAR tools</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-Debug-Mailbox-with-IAR-tools/m-p/2031938#M57570</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245663"&gt;@rony243&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;The ERR_ISP_PARAM_ERROR return code indicates that there is an issue with the parameters of the Unlock command you are sending. On the LPC54605, the Unlock command expects a specific set of conditions to be met. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;Harry&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jan 2025 03:39:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-Debug-Mailbox-with-IAR-tools/m-p/2031938#M57570</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-01-22T03:39:41Z</dc:date>
    </item>
  </channel>
</rss>