<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S28: PUF_GetHwKey fails when using prince region0</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027476#M57520</link>
    <description>Hi, thanks Alice for the reply I am using MCUXpresso Secure Provisioning Tool.&lt;BR /&gt;Some more details I should have added from the start. The application I am using is split i 2 parts one bootloader and one application. I right now load the bootloader using MCUXpresso Secure Provisioning and works as expected. But later when the devie is booted and in the bootloader mode i need to be able to load the application. What steps do i need to take to achieve the following unlock memory area i want write application to , flash application and encrypt the newly written area?&lt;BR /&gt;</description>
    <pubDate>Tue, 14 Jan 2025 09:28:49 GMT</pubDate>
    <dc:creator>tobias91</dc:creator>
    <dc:date>2025-01-14T09:28:49Z</dc:date>
    <item>
      <title>LPC55S28: PUF_GetHwKey fails when using prince region0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2024864#M57492</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;trying to set up secure boot on a LPC55S28 custom board. Following along the prince example from the SDK. Only using prince region 0. boot type is Encrypted (Prince) and signed&lt;BR /&gt;When i get to this part of the example:&lt;BR /&gt;&lt;BR /&gt;status = FFR_KeystoreGetKC(&amp;amp;g_iap.config, &amp;amp;keyCode[0], kFFR_KeyTypePrinceRegion0);&lt;BR /&gt;&lt;BR /&gt;status = PUF_GetHwKey(PUF, keyCode, sizeof(keyCode), kPUF_KeySlot2, rand());&lt;/P&gt;&lt;P&gt;The FFR_KeystoreGetKC return key and status okay but PUF_GetHwKey always fails. What am I missing? Something more in the secure provisioning tool for CMPA/CFPA I need to set up?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 13:27:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2024864#M57492</guid>
      <dc:creator>tobias91</dc:creator>
      <dc:date>2025-01-09T13:27:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28: PUF_GetHwKey fails when using prince region0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027458#M57519</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231400"&gt;@tobias91&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="times new roman,times" size="3"&gt;&lt;SPAN&gt;If you want to use the Secure boot + PRINCE function, I highly recommend that you use MCUXpresso Secure Provisioning too. Refer to "6.4.3.3 Booting signed or PRINCE encrypted image" in &amp;lt;MCUXpresso Secure Provisioning Tool User Guide&amp;gt;.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="times new roman,times" size="3"&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT face="times new roman,times" size="3"&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jan 2025 09:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027458#M57519</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-01-14T09:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28: PUF_GetHwKey fails when using prince region0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027476#M57520</link>
      <description>Hi, thanks Alice for the reply I am using MCUXpresso Secure Provisioning Tool.&lt;BR /&gt;Some more details I should have added from the start. The application I am using is split i 2 parts one bootloader and one application. I right now load the bootloader using MCUXpresso Secure Provisioning and works as expected. But later when the devie is booted and in the bootloader mode i need to be able to load the application. What steps do i need to take to achieve the following unlock memory area i want write application to , flash application and encrypt the newly written area?&lt;BR /&gt;</description>
      <pubDate>Tue, 14 Jan 2025 09:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027476#M57520</guid>
      <dc:creator>tobias91</dc:creator>
      <dc:date>2025-01-14T09:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S28: PUF_GetHwKey fails when using prince region0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027538#M57522</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231400"&gt;@tobias91&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It seems the same issue with your private ticket. I have reply you on that, please check it. Thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jan 2025 10:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S28-PUF-GetHwKey-fails-when-using-prince-region0/m-p/2027538#M57522</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2025-01-14T10:37:11Z</dc:date>
    </item>
  </channel>
</rss>