<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54628 GT911 Touch controller not ACK</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-GT911-Touch-controller-not-ACK/m-p/2017473#M57442</link>
    <description>&lt;P&gt;It turns out that the display on my board does not use the GT911 touch controller but actually the FT5336 chip.&amp;nbsp; Just had to change the&amp;nbsp;&lt;SPAN&gt; DEMO_PANEL define to DEMO_PANEL_RK043FN02H and all works fine now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 19 Dec 2024 22:13:26 GMT</pubDate>
    <dc:creator>samv</dc:creator>
    <dc:date>2024-12-19T22:13:26Z</dc:date>
    <item>
      <title>LPC54628 GT911 Touch controller not ACK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-GT911-Touch-controller-not-ACK/m-p/2017423#M57441</link>
      <description>&lt;P&gt;I am trying to run the lcxpresso54628_lvgl_guider demo on the OM13098UL dev. board.&lt;/P&gt;&lt;P&gt;It compiles but crashes when run at the "&lt;SPAN&gt;status = GT911_Init(&amp;amp;s_touchHandle, &amp;amp;s_touchConfig);" line.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Here is the message:&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Touch IC initialization failed&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;ASSERT ERROR " false ": file "lvgl_support.c" Line "444" function name "DEMO_InitTouch"&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The I2C lines do send out the touch controller address of 0x5D but there is no ACK so the check fails and program breaks.&amp;nbsp;&amp;nbsp;Other demos cause the same issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;The original demo that came with the dev. board ran fine and I would like to reload it and look at the I2C lines to see any difference.&amp;nbsp; Where can I get that hex file to upload to the board?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sam&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 19:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-GT911-Touch-controller-not-ACK/m-p/2017423#M57441</guid>
      <dc:creator>samv</dc:creator>
      <dc:date>2024-12-19T19:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54628 GT911 Touch controller not ACK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-GT911-Touch-controller-not-ACK/m-p/2017473#M57442</link>
      <description>&lt;P&gt;It turns out that the display on my board does not use the GT911 touch controller but actually the FT5336 chip.&amp;nbsp; Just had to change the&amp;nbsp;&lt;SPAN&gt; DEMO_PANEL define to DEMO_PANEL_RK043FN02H and all works fine now.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 22:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-GT911-Touch-controller-not-ACK/m-p/2017473#M57442</guid>
      <dc:creator>samv</dc:creator>
      <dc:date>2024-12-19T22:13:26Z</dc:date>
    </item>
  </channel>
</rss>