<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Driving  a 0603 LED by LPC5516 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2013908#M57409</link>
    <description>&lt;P&gt;As a general practice on STM32 or PIC18,Is that possible to drive a green or red&amp;nbsp; LED by GPIO from LPC5516, plus a resistor on the IO pin?&lt;/P&gt;</description>
    <pubDate>Sun, 15 Dec 2024 08:57:58 GMT</pubDate>
    <dc:creator>uzslm</dc:creator>
    <dc:date>2024-12-15T08:57:58Z</dc:date>
    <item>
      <title>Driving  a 0603 LED by LPC5516</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2013908#M57409</link>
      <description>&lt;P&gt;As a general practice on STM32 or PIC18,Is that possible to drive a green or red&amp;nbsp; LED by GPIO from LPC5516, plus a resistor on the IO pin?&lt;/P&gt;</description>
      <pubDate>Sun, 15 Dec 2024 08:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2013908#M57409</guid>
      <dc:creator>uzslm</dc:creator>
      <dc:date>2024-12-15T08:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: Driving  a 0603 LED by LPC5516</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2013971#M57411</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It is dependent on the current the LED has to consume to light up the LED.&lt;/P&gt;
&lt;P&gt;The GPIO pin of LPC5516 can provide 4mA current, if 4mA current can light up the LED, it is okay, you can connect a serial resistor (3.3V-0.7V)/4mA=650 ohm to limit the current.&lt;/P&gt;
&lt;P&gt;If the 4mA is not enough to light up the LED, pls connect a transistor.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1734313869744.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315919i79418F92F8524EE0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1734313869744.png" alt="xiangjun_rong_0-1734313869744.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;copied from data sheet of LPC551x.&lt;/P&gt;
&lt;P&gt;AS the above table, both the source/sink current of each GPIO is 4mA.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 01:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2013971#M57411</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-12-16T01:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: Driving  a 0603 LED by LPC5516</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2014777#M57421</link>
      <description>&lt;P&gt;&lt;SPAN&gt;XiangJun,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you for all the information!&lt;/P&gt;&lt;P&gt;I had similar LEDs as indicators working on my previous boards,i would like to check their current to decide how muck ohms for the resistors,hope that 1k can be okay.&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;uzslm&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 00:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Driving-a-0603-LED-by-LPC5516/m-p/2014777#M57421</guid>
      <dc:creator>uzslm</dc:creator>
      <dc:date>2024-12-17T00:59:01Z</dc:date>
    </item>
  </channel>
</rss>