<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC824 Invert Input Signal to Output in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Invert-Input-Signal-to-Output/m-p/2009511#M57367</link>
    <description>&lt;P&gt;Using the LPC824 Is there an efficient way to take an input signal on a pin, invert it and route/output it on another pin without using an interrupt?&lt;/P&gt;</description>
    <pubDate>Sat, 07 Dec 2024 19:20:49 GMT</pubDate>
    <dc:creator>scruffmeister</dc:creator>
    <dc:date>2024-12-07T19:20:49Z</dc:date>
    <item>
      <title>LPC824 Invert Input Signal to Output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Invert-Input-Signal-to-Output/m-p/2009511#M57367</link>
      <description>&lt;P&gt;Using the LPC824 Is there an efficient way to take an input signal on a pin, invert it and route/output it on another pin without using an interrupt?&lt;/P&gt;</description>
      <pubDate>Sat, 07 Dec 2024 19:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Invert-Input-Signal-to-Output/m-p/2009511#M57367</guid>
      <dc:creator>scruffmeister</dc:creator>
      <dc:date>2024-12-07T19:20:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC824 Invert Input Signal to Output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Invert-Input-Signal-to-Output/m-p/2009767#M57370</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;
&lt;P&gt;I have not good idea to invert a signal from a pad and output an inverted signal to another pad without interrupt for LPC824.&lt;/P&gt;
&lt;P&gt;But the LPC804 has PLU, which enable you invert a signal from the PLU input pad and output the inverted signal to another PLU output pad.&lt;/P&gt;
&lt;P&gt;This is LPC804 website:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc800-arm-cortex-m0-plus-/lpc800-32-bit-arm-cortex-m0-plus-based-low-cost-mcu:LPC80X" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc800-arm-cortex-m0-plus-/lpc800-32-bit-arm-cortex-m0-plus-based-low-cost-mcu:LPC80X&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Of course, you can use PINT module to generate interrupt, in the ISR, read the logic of input pin, and output the inverted&amp;nbsp; logic to another GPIO pad.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 07:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Invert-Input-Signal-to-Output/m-p/2009767#M57370</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-12-09T07:00:47Z</dc:date>
    </item>
  </channel>
</rss>